Dear Sir,
i have one question about the pairing between different interface.
Can the Max9271(Serializer, Parallel to GMSL) be paired with Max97614(Deserializer, GMSL to MIPI)? Thanks!
BRs,
Tim
MAX9271
Production
The MAX9271 compact serializer is designed to drive 50O coax or 100O shielded twisted-pair (STP) cable. The device pairs with the MAX9272 deserializer...
Datasheet
MAX9271 on Analog.com
MAX967
Production
The MAX965–MAX970 single/dual/quad micropower
comparators feature rail-to-rail inputs and outputs, and
fully specified single-supply operation down to...
Datasheet
MAX967 on Analog.com
Dear Sir,
i have one question about the pairing between different interface.
Can the Max9271(Serializer, Parallel to GMSL) be paired with Max97614(Deserializer, GMSL to MIPI)? Thanks!
BRs,
Tim
Hi Max96714 ,
This forum is for reference designs and Circuits from the Lab. It looks like the GMSL devices are not directly supported on EngineerZone yet, there is some guidance on how to get support for GMSL products in this thread:
-Mark
Hi Max96714 ,
This forum is for reference designs and Circuits from the Lab. It looks like the GMSL devices are not directly supported on EngineerZone yet, there is some guidance on how to get support for GMSL products in this thread:
-Mark