We are using CN0566 with 21R2 SD CARD image and experiencing the following error when running the receiverDataCollection.m example code:
Error using matlabshared.libiio.base/cstatusid
Failed to find device: one-bit-adc-dac.
Error in matlabshared.libiio.base/getDev
Error in adi.internal.AXICorePlutoTDD/setupInit (line 386)
obj.GPIODevIIO = obj.getDev('one-bit-adc-dac');
Error in adi.PlutoTDD/setupInit (line 58)
setupInit@adi.internal.AXICorePlutoTDD(obj);
Error in adi.PlutoTDD/setupImpl (line 53)
setupInit(obj);
Error in setupTddEngine (line 7)
bf_TDD();
Error in setupAntenna (line 16)
bf_TDD = setupTddEngine();
Error in findTxFrequency (line 21)
[rx,bf,~,tx,bf_TDD] = setupAntenna(f_start);
Error in receiverDataCollection (line 26)
fc_hb100 = findTxFrequency();
>> which matlabshared.libiio.base
C:\ProgramData\MATLAB\SupportPackages\R2023b\toolbox\shared\libiio\base\+matlabshared\+libiio\base.p % matlabshared.libiio.base constructor
>>
Is this a known issue? Is this error due to version issue? Please suggest.