I recently purchased an EVAL-AD5941BATZ kit for EIS measurement and intend to use it with sensorpal but am confused with the wording for DC Bias as one of the parameters. Does DC bias refer to a DC bias on top of the AC perturbation or is it the open circuit voltage of the battery I'm using as a test? The use of mVpp is also confusing as it relates to DC bias because in other notes and questions, DC voltage has been said to go up to 2.4V while the limit here is 1200mVpp
RE: Software operation of battery impedance spectrum measurement
Maybe a more succinct question would be what I would set DC bias to if I wanted to test a 3.7V battery just using the board and as described in the the user guide.
Thank you