Post Go back to editing

Where shall I get mechanical dimensions of MAX30003 and MAX86171? They are not available in datasheet.

Thread Summary

The user sought package details and mechanical dimensions for a device, which were found in the 'Package Information' section of the MAX30003 datasheet (page 45) and the MAX86171 datasheet (page 3). The final answer also directed the user to post such questions in the appropriate product technology forums for better support.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX30003, MAX86171

The data sheet covers technical details containing electrical and electronics only. I am not able to find the package details, mechanical dimensions. Please share document where these information are included.

Parents
  • FormerMember
    FormerMember
on Sep 22, 2023 9:37 AM
0

When I checked the datasheet for the MAX30003, there is a section towards the back of the document called "Package Information" (page 45), and there are links out to the package dimension there based on which package you are using.  I found the same section in the MAX86171 datasheet on page 3.  Hope this helps.

PS - This forum is dedicated for questions about the different Analog Devices reference designs and Circuits from the Lab designs, so I the future please post these types of questions in the correct product technology forums.  Thanks.

Cheers,

Brandon

Reply
  • FormerMember
    FormerMember
on Sep 22, 2023 9:37 AM
0

When I checked the datasheet for the MAX30003, there is a section towards the back of the document called "Package Information" (page 45), and there are links out to the package dimension there based on which package you are using.  I found the same section in the MAX86171 datasheet on page 3.  Hope this helps.

PS - This forum is dedicated for questions about the different Analog Devices reference designs and Circuits from the Lab designs, so I the future please post these types of questions in the correct product technology forums.  Thanks.

Cheers,

Brandon

Children
No Data