i made connections of rs485 and cn0359 as per intrsutcted,and i am using putty, I entered command ‘100 poll’, 100 poll’\n’, 100poll, I tried many ways but the address in the Cn0359 does not set to 100, i changed address manually to 84 and I tried multiple commands to set frequency/ voltage, with 84 setfreq 120.6 etc but nothing works, it does not set any frequency in device and i dont receive any intput from device as well. i made putty connection with CR/LF on and local echo and line editing, i also checked signals at v+ and - which is square but at A/B i am not getting any signal/ probably its high and when i sent a command it goes low for an instance. but still even after this the device does not take and input. i tried command "84 poll" 84 setfreq 120.9 "84 setfreq 120.0'\n' and many variations nothing works. kindly help
Could you please look into it and address the issue.
And I could not find any command to FETCH the conductivity values from the CN0359 to PC, all the commands are given to SET the values in CN0359. But our major goal is to set and fetch the values from the board. Could you please suggest a solution for this. I have checked for a solution in engineerZone, and it doesn’t give any solution for my problem. Kindly help us solve this. If possible, we can set up a meeting whenever is feasible to you, so that it would be easy to communicate and solve the issue. Awaiting your response.
i made putty connection with CR/LF on and local echo and line editing, i also checked signals at v+ and - which is square but at A/B i am not getting any signal/ probably its high and when i sent a command it goes low for an instance. but still even after this the device does not take and input. i tried command "84 poll" 84 setfreq 120.9 "84 setfreq 120.0'\n' and many variations nothing works. kindly help
[edited by: pranavreddy at 9:56 PM (GMT -4) on 10 Aug 2023]