Post Go back to editing

EVAL-ADICUP3029 & EVAL-AD5941BATZ, AD5940_BATImpedance Problems

Thread Summary

The user encountered incorrect impedance measurement data when using the BATImpedance library with the EVAL-AD5941BATZ kit and IAR. The excitation signal stops after 9 seconds due to the sweep configuration, which limits the measurement to 101 sweep points. The final answer suggests checking the `AppBATCfg.NumOfData` value, which should be set to `-1` for continuous measurements, and adjusting the `PwrMod` setting for frequencies above 80kHz. The user also noted that switching to the AD5940/41ELCZ kit resolved similar issues.
AI Generated Content
Category: Software
Product Number: EVAL-ADICUP3029 & EVAL-AD5941BATZ [45891791]

Hi,

After having successfully tested the EVAL-AD5941BATZ kit with the SensorPal software, I wanted to use the BATImpedance library from the GitHub platform to compile with IAR. I manage to compile but when I read the data they are apparently wrong :

The data :

Freq: 1.000000 (real, image) = ,37.162163 , -152.027023 ,mOhm
Freq: 1.247089 (real, image) = ,-206.896545 , 567.241394 ,mOhm
Freq: 1.555230 (real, image) = ,261.538452 , 157.692307 ,mOhm
Freq: 1.939510 (real, image) = ,-63.793106 , -284.482758 ,mOhm
Freq: 2.418741 (real, image) = ,15.000001 , 45.000000 ,mOhm
Freq: 3.016385 (real, image) = ,-46.153847 , 5.769231 ,mOhm
Freq: 3.761699 (real, image) = ,115.000000 , -45.000000 ,mOhm
Freq: 4.691173 (real, image) = ,-94.000000 , 12.000000 ,mOhm
Freq: 5.850308 (real, image) = ,-115.000000 , -205.000000 ,mOhm
Freq: 7.295854 (real, image) = ,-14.705883 , -41.176472 ,mOhm
Freq: 9.098577 (real, image) = ,-266.666687 , 133.333344 ,mOhm
Freq: 11.346732 (real, image) = ,-29.039303 , -7.205240 ,mOhm
Freq: 14.150382 (real, image) = ,-7.692308 , 88.461533 ,mOhm
Freq: 17.646782 (real, image) = ,0.000000 , -50.000000 ,mOhm
Freq: 22.007103 (real, image) = ,50.000000 , -50.000000 ,mOhm
Freq: 27.444809 (real, image) = ,-134.615387 , 273.076904 ,mOhm
Freq: 34.226112 (real, image) = ,50.000000 , -50.000000 ,mOhm
Freq: 42.682995 (real, image) = ,66.666672 , 0.000000 ,mOhm
Freq: 53.229485 (real, image) = ,46.341465 , -17.073172 ,mOhm
Freq: 66.381889 (real, image) = ,33.823528 , 39.705883 ,mOhm
Freq: 82.784103 (real, image) = ,66.666672 , -8.333334 ,mOhm
Freq: 103.239120 (real, image) = ,75.000000 , -275.000000 ,mOhm
Freq: 128.748337 (real, image) = ,-9.756097 , -12.195122 ,mOhm
Freq: 160.560593 (real, image) = ,0.000000 , 100.000000 ,mOhm
Freq: 200.233307 (real, image) = ,102.439026 , 28.048780 ,mOhm
Freq: 249.708694 (real, image) = ,66.853935 , -26.966291 ,mOhm
Freq: 311.408905 (real, image) = ,-200.000000 , 150.000000 ,mOhm
Freq: 388.354523 (real, image) = ,0.000000 , 30.000002 ,mOhm
Freq: 484.312531 (real, image) = ,-10.955056 , -47.471912 ,mOhm
Freq: 603.980713 (real, image) = ,41.176472 , 14.705883 ,mOhm
Freq: 753.217529 (real, image) = ,-68.918922 , 63.513512 ,mOhm
Freq: 939.329041 (real, image) = ,-73.076920 , 15.384616 ,mOhm
Freq: 1171.426636 (real, image) = ,-1.621622 , -30.270269 ,mOhm
Freq: 1460.872925 (real, image) = ,-72.602737 , 60.273975 ,mOhm
Freq: 1821.838135 (real, image) = ,92.920349 , -6.194690 ,mOhm
Freq: 2271.993896 (real, image) = ,-31.034481 , 222.413803 ,mOhm
Freq: 2833.377930 (real, image) = ,-12.500000 , -25.000000 ,mOhm
Freq: 3533.473633 (real, image) = ,3.503185 , -1.910828 ,mOhm
Freq: 4406.554688 (real, image) = ,-27.358490 , 20.754717 ,mOhm
Freq: 5495.364746 (real, image) = ,-110.000000 , -180.000000 ,mOhm
Freq: 6853.207520 (real, image) = ,55.882351 , 26.470589 ,mOhm
Freq: 8546.557617 (real, image) = ,-60.000004 , 30.000002 ,mOhm
Freq: 10658.315430 (real, image) = ,-63.414635 , 20.731707 ,mOhm
Freq: 13291.865234 (real, image) = ,6.234414 , 24.688280 ,mOhm
Freq: 16576.134766 (real, image) = ,150.000000 , 50.000000 ,mOhm
Freq: 20671.910156 (real, image) = ,25.000000 , 25.000000 ,mOhm
Freq: 25779.707031 (real, image) = ,58.620689 , 3.448276 ,mOhm
Freq: 32149.580078 (real, image) = ,-38.461540 , 7.692308 ,mOhm
Freq: 40093.378906 (real, image) = ,13.461539 , 17.307693 ,mOhm
Freq: 50000.000000 (real, image) = ,39.285713 , 32.142857 ,mOhm


Here are the settings :

AppBATCfg_Type *pBATCfg;

AppBATGetCfg(&pBATCfg);
pBATCfg->SeqStartAddr = 0;
pBATCfg->MaxSeqLen = 512;
pBATCfg->RcalVal = 50.0; /* Value of RCAL on EVAL-AD5941BATZ board is 50mOhm */
pBATCfg->ACVoltPP = 300.0f; /* Pk-pk amplitude is 300mV */
pBATCfg->DCVolt = 1200.0f; /* Offset voltage of 1.2V*/
pBATCfg->DftNum = DFTNUM_8192;

pBATCfg->FifoThresh = 2; /* 2 results in FIFO, real and imaginary part. */

pBATCfg->SinFreq = 200; /* Sin wave frequency. THis value has no effect if sweep is enabled */

pBATCfg->SweepCfg.SweepEn = bTRUE; /* Set to bTRUE to enable sweep function */
pBATCfg->SweepCfg.SweepStart = 1.0f; /* Start sweep at 1Hz */
pBATCfg->SweepCfg.SweepStop = 50000.0f; /* Finish sweep at 1000Hz */
pBATCfg->SweepCfg.SweepPoints = 50; /* 100 frequencies in the sweep */
pBATCfg->SweepCfg.SweepLog = bTRUE; /* Set to bTRUE to use LOG scale. Set bFALSE to use linear scale */

When I check the excitation signal after a reset, it goes out after 9 seconds. For what? If the measurements are made without the excitation, normally they will be wrong. Do you know what can cause this error?

Thanks in advance.

Parents
  • Hi,

    The same code in Github is used for Sensorpal. May I know if you have checked the github firmware on EVAL-AD5940BATZ kit?

    If AppBATCfg.NumOfData is not -1,but set to "n",  measurement is done only for "n" complete frequency sweeps (i.e., from  sweepstart till sweepstop n times) after which it stops.

  • Hi

    The definition of the default configuration structure and this one:

    AppBATCfg_Type AppBATCfg =
    {

    . state = STATE_IDLE,
    .bParaChanged = bFALSE,

    . SeqStartAddr = 0,
    . MaxSeqLen = 0,

    . SeqStartAddrCal = 0,
    . MaxSeqLenCal = 0,

    . SysClkFreq = 16000000.0,
    . WuptClkFreq = 32000.0,
    . AdcClkFreq = 16000000.0,
    . BatODR = 20,0, /* 20,0 Hz*/
    . numOfData = -1, <-- not modified.

    . PwrMod = AFEPWR_LP,
    . ACVoltPP = 800,0,
    . DCVolt = 1100.0f,
    . SinFreq = 50000.0, /* 50kHz */
    . RcalVal = 50.0, /* 50mOhm */

    . ADCSinc3Osr = ADCSINC3OSR_4,
    . ADCSinc2Osr = ADCSINC2OSR_22,

    . DftNum = DFTNUM_16384,
    . DftSrc = DFTSRC_SINC3,
    . HanWinEn = bTRUE,

    . FifoThresh = 4,
    . BATInited = bFALSE,
    . StopRequired = bFALSE,
    . MeasSeqCycleCount = 0,

    . SweepCfg.SweepEn = bTRUE,
    . SweepCfg.SweepStart = 1000,
    . SweepCfg.SweepStop = 100000.0,
    . SweepCfg.SweepPoints = 101,
    . SweepCfg.SweepLog = bFALSE,
    . SweepCfg.SweepIndex = 0,

    };

    I don't see where, apart from the configuration I provided earlier, can change the numOfData value.

    Why does the excitation signal not continue despite the continuous calibration and measurement process?

    I will continue to investigate and if you have a solution, it will be with pleasure.

    Thanks.

  • same problem here!

    This is Exactly what I am getting from my board! 

    dear Volotek would you please help me if you could solve the problem?

    I have been dealing with this problem for a long time.

  • Hi,

    The excitation signal goes out after 9 seconds because when sweep is enabled, excitation is given for 101 sweep points after which measurement and excitation stops and results are displayed.

    Also Note:

    For excitation frequencies below 80kHz,

    . PwrMod = AFEPWR_LP,

    For exciation frequencies above 80kHz, 

    . PwrMod = AFEPWR_HP,

    You may refer to (+) SensorPal Battery impedance measurement - Q&A - Reference Designs - EngineerZone (analog.com)

  • Thanks for your precisions. We continue to do tests.

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.