Post Go back to editing

AD5421:在中文参考电路中引脚LOOP-接稳压二极管的负极,英文数据手册中接LOOP-接稳压二极管的正极,想问一下怎么样接正确 Translate: In the Chinese reference circuit, the pin LOOP is connected to the negative pole of the Zener diode, and in the English data sheet, the pin LOOP is connected to the positive pole

Category: Hardware
Product Number: AD5421

Translate: 

AD5421: In the Chinese reference circuit, pin LOOP-connects to the negative pole of the Zener diode,
and in the English data sheet connects LOOP-to the positive pole of the Zener diode. I would like to
ask how to connect it correctly AD5421: In the Chinese reference circuit, pin LOOP-connects to the
negative pole of the Zener diode, and in the English data sheet connects LOOP-to the positive pole of the Zener diode.
I would like to ask how to connect it correctly

AD5421:在中文参考电路中引脚LOOP-接稳压二极管的负极,英文数据手册中接LOOP-接稳压二极管的正极,想问一下怎么样接正确



Translated
[edited by: GenevaCooper at 1:49 PM (GMT -4) on 23 May 2023]
Parents
  • Hi SantaTyr,

    It looks like the Chinese version is NOT correct. Refer to the AD5421 datasheet text on page 32:

    " If it is possible that the voltage at LOOP− may be forced positive with respect to COM, or if the voltage difference between LOOP− and COM may be forced in excess of 5 V, a 4.7 V low leakage Zener diode should be placed between COM and the LOOP− pin, as shown in Figure 50, to protect the AD5421 from potential damage. "

    I'll inquire about updating the Chinese CN0382 document.

    -Mark

Reply
  • Hi SantaTyr,

    It looks like the Chinese version is NOT correct. Refer to the AD5421 datasheet text on page 32:

    " If it is possible that the voltage at LOOP− may be forced positive with respect to COM, or if the voltage difference between LOOP− and COM may be forced in excess of 5 V, a 4.7 V low leakage Zener diode should be placed between COM and the LOOP− pin, as shown in Figure 50, to protect the AD5421 from potential damage. "

    I'll inquire about updating the Chinese CN0382 document.

    -Mark

Children
No Data