Post Go back to editing

CN0511 code issue

Category: Software
Product Number: CN0511
Software Version: Git master

I think this page just needs to be removed (it’s not used anywhere, and is duplicated on the next page).

https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0511/libad9166-iio_installations

 

This page:

https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0511

 

includes:

Once the next version of Analog Devices Kuiper Linux gets released (2021_R2), these steps will be removed.

(I think that has happened now?) What’s the update?

 

The Python uses register reads/writes to access temperature?

https://github.com/analogdevicesinc/pyadi-iio/blob/master/adi/ad9166.py#L92-L108

 

I don’t understand that at all – since the driver exposes that as an IIO attribute.

https://wiki.analog.com/resources/tools-software/linux-drivers/iio-pll/ad9162#read_temperature

 

 

and NCO:

               https://github.com/analogdevicesinc/pyadi-iio/blob/master/adi/ad9166.py#L125-L134

               https://github.com/analogdevicesinc/pyadi-iio/blob/master/adi/ad9166.py#L136-L145

 

which is also supported by the driver:

https://wiki.analog.com/resources/tools-software/linux-drivers/iio-pll/ad9162#change_nco_frequency

 

same for the FIR85 – implemented with reg read/write:

https://github.com/analogdevicesinc/pyadi-iio/blob/master/adi/ad9166.py#L146-L166

 

but also in the driver:

https://wiki.analog.com/resources/tools-software/linux-drivers/iio-pll/ad9162#enable_fir85_filter1

 

Is there something wrong with the driver that we shouldn’t be using it?