Post Go back to editing

CN0540/DE10-nano signal wrong

Category: Hardware
Product Number: CN0540/DE10-nano

Hi,

I use the cn0540 with de10-nano to connect data below. The DS1(Power), DS2(fault) and DS4(CC) are on. 

I connect the vibrating IEPE sensor to SMA or connect signal source with voltage amplitude of 1V to VIN (P10 disconnected). However, with the help of iio-oscilloscope, the plot seems that the board only has noise and can not collect the sensor data.

I tentatively infer that there are some error in switch ADG5421 and test the connection and disconnection of some nodes.

According to schematic diagram below, i find R61 left node is not connected to R10 up node but R61 right node is connected to R10 up node. So i infer that ADG5421 is broken. Is it right?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.