Added Category
[edited by: GenevaCooper at 2:01 PM (GMT -5) on 5 Jan 2023]
AD7746
Production
The AD7745/AD7746 are a high resolution, S-? capacitance-to-digital converter (CDC). The capacitance to be measured is connected directly to the device...
Datasheet
AD7746 on Analog.com
Hi lkxaaa ,
I will be moving this thread to the proper forum. I hope someone from the community can assist you.
Regards,
JC
Hi Ikxaaa,
The No-OS drivers are a set of functions, registers and parameters that we provide to facilitate the programming of the device (in your case the AD7746) for any microcontroller. The No-OS drivers…
Hi Ikxaaa,
The provided No-OS drivers are available for the following platforms. If you do not use any of those platforms you will problably need to modify the No-OS drivers:
In the following link you…
1. Yes
2.CIN1_POS=CIN1(+)
CIN1_NEG=CIN1(-)
CIN2_POS=CIN2(+)
CIN2_NEG=CIN2(-)
Is the INT pin in CN0552 equivalent to the RDY pin in the AD7746?
yes.
Sorry, haven't seen the message lately.
When I measure capacitance with CN0552, the capacitance value is 1pF that is right.
but When I added my previous part of the circuit, the capacitance value became 4pF and three capacitor values appear at once.
Measure the capacitance value as shown in the figure.
In actual measurements, the X of U2 is connected to the ACCA pin; The X of U3 is CIN1_POS pin.
Hi lkxaaa,
Note that a typical 74HC4051 has pin capacitances well above 4 pF:
-Mark
This is a question that I need to think about again.
I also want to ask what is the formula for converting the data read from the capacitance data registers into the capacitor value.
Most of the programs in this part are consistent, but the later conversion of the read data into the actual capacitance value, the formula is different, can you give me some guidance.
for example:
I haven't found a pattern that I would like you to guide me
Thanks.
This is a question that I need to think about again.
I also want to ask what is the formula for converting the data read from the capacitance data registers into the capacitor value.
Most of the programs in this part are consistent, but the later conversion of the read data into the actual capacitance value, the formula is different, can you give me some guidance.
for example:
I haven't found a pattern that I would like you to guide me
Thanks.
From the datasheet description of the 24-bit cap data register:
The 0x000000 code represents negative full scale (–4.096 pF), the 0x800000 code represents zero scale (0 pF), and the 0xFFFFFF code represents positive full scale (+4.096 pF).
This is offset binary. You can subtract 0x800000 first, which will result in a signed, 2s complement number. Be careful that the sign extension is done properly if you are using a 32-bit word.
then multiply the result by the value of one lsb, which would be 4.096 pF / 8388608
It is a good idea to double-check your math by passing known values to it, and make sure it returns the expected result. (for example, sending digital code zero, 0x800000, 0xFFFFFF should return -4.096, 0, and 4.096, respectively.
-Mark
hi,Mark
I tried your suggestion today and still don't get the results I want.
this is my head file.
// I2Cdev library collection - AD7746 I2C device class header file // Based on Analog Devices AD7746 Datasheet, Revision 0, 2005 // 2012-04-01 by Peteris Skorovs <pskorovs@gmail.com> // // This I2C device library is using (and submitted as a part of) Jeff Rowberg's I2Cdevlib library, // which should (hopefully) always be available at https://github.com/jrowberg/i2cdevlib // // Changelog: // 2012-04-01 - initial release /* ============================================ I2Cdev device library code is placed under the MIT license Copyright (c) 2012 Peteris Skorovs Permission is hereby granted, free of charge, to any person obtaining a copy of this software and associated documentation files (the "Software"), to deal in the Software without restriction, including without limitation the rights to use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of the Software, and to permit persons to whom the Software is furnished to do so, subject to the following conditions: The above copyright notice and this permission notice shall be included in all copies or substantial portions of the Software. THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE. =============================================== */ #ifndef _AD7746_H_ #define _AD7746_H_ #include "I2Cdev.h" #define AD7746_ADDRESS 0x48 #define AD7746_DEFAULT_ADDRESS AD7746_ADDRESS #define AD7746_RA_STATUS 0x00 // Status #define AD7746_RA_CAP_DATA_H 0x01 // Cap data #define AD7746_RA_CAP_DATA_M 0x02 // Cap data #define AD7746_RA_CAP_DATA_L 0x03 // Cap data #define AD7746_RA_VT_DATA_H 0x04 // VT data #define AD7746_RA_VT_DATA_M 0x05 // VT data #define AD7746_RA_VT_DATA_L 0x06 // VT data #define AD7746_RA_CAP_SETUP 0x07 // Cap Setup #define AD7746_RA_VT_SETUP 0x08 // VT Setup #define AD7746_RA_EXC_SETUP 0x09 // Exc Setup #define AD7746_RA_CONFIGURATION 0x0A // Configuration #define AD7746_RA_CAP_DAC_A 0x0B // Cap DAC A #define AD7746_RA_CAP_DAC_B 0x0C // Cap DAC B #define AD7746_RA_CAP_OFF_H 0x0D #define AD7746_RA_CAP_OFF_L 0x0E #define AD7746_RA_CAP_GAIN_H 0x0F #define AD7746_RA_CAP_GAIN_L 0x10 #define AD7746_RA_VOLT_GAIN_H 0x11 #define AD7746_RA_VOLT_GAIN_L 0x12 #define AD7746_RESET 0xBF // Status #define AD7746_EXCERR_BIT 3 #define AD7746_RDY_BIT 2 #define AD7746_RDYVT_BIT 1 #define AD7746_RDYCAP_BIT 0 // Cap Setup #define AD7746_CAPEN_BIT 7 #define AD7746_CIN2_BIT 6 #define AD7746_CAPDIFF_BIT 5 #define AD7746_CACHOP_BIT 0 #define AD7746_CAPEN (1 << AD7746_CAPEN_BIT) #define AD7746_CIN2 (1 << AD7746_CIN2_BIT) // VT Setup #define AD7746_VTEN_BIT 7 #define AD7746_VTMD_BIT_1 6 #define AD7746_VTMD_BIT_0 5 #define AD7746_EXTREF_BIT 4 #define AD7746_VTSHORT_BIT 1 #define AD7746_VTCHOP_BIT 0 #define AD7746_VTEN (1 << AD7746_VTEN_BIT) #define AD7746_VTMD_INT_TEMP 0 #define AD7746_VTMD_EXT_TEMP (1 << AD7746_VTMD_BIT_0) #define AD7746_VTMD_VDD_MON (1 << AD7746_VTMD_BIT_1) #define AD7746_VTMD_VIN (1 << AD7746_VTMD_BIT_1) | (1 << AD7746_VTMD_BIT_0) // Exc Setup #define AD7746_CLKCTRL_BIT 7 #define AD7746_EXCON_BIT 6 #define AD7746_EXCB_BIT 5 #define AD7746_INV_EXCB_BIT 4 #define AD7746_EXCA_BIT 3 #define AD7746_INV_EXCA_BIT 2 #define AD7746_EXCLVL_BIT_1 1 #define AD7746_EXCLVL_BIT_0 0 #define AD7746_EXCA (1 << AD7746_EXCA_BIT) #define AD7746_EXCB (1 << AD7746_EXCB_BIT) #define AD7746_EXCON (1 << AD7746_EXCON_BIT) #define AD7746_EXCLVL_VDD_X_1_8 0 #define AD7746_EXCLVL_VDD_X_1_4 (1 << AD7746_EXCLVL_BIT_0) #define AD7746_EXCLVL_VDD_X_3_8 (1 << AD7746_EXCLVL_BIT_1) #define AD7746_EXCLVL_VDD_X_1_2 (1 << AD7746_EXCLVL_BIT_1) | (1 << AD7746_EXCLVL_BIT_0) // Configuration #define AD7746_VTF_BIT_1 7 #define AD7746_VTF_BIT_0 6 #define AD7746_CAPF_BIT_2 5 #define AD7746_CAPF_BIT_1 4 #define AD7746_CAPF_BIT_0 3 #define AD7746_MD_BIT_2 2 #define AD7746_MD_BIT_1 1 #define AD7746_MD_BIT_0 0 #define AD7746_VTF_20P1 0 #define AD7746_VTF_32P1 (1 << AD7746_VTF_BIT_0) #define AD7746_VTF_62P1 (1 << AD7746_VTF_BIT_1) #define AD7746_VTF_122P1 (1 << AD7746_VTF_BIT_1) | (1 << AD7746_VTF_BIT_0) #define AD7746_CAPF_11P0 0 #define AD7746_CAPF_11P9 (1 << AD7746_CAPF_BIT_0) #define AD7746_CAPF_20P0 (1 << AD7746_CAPF_BIT_1) #define AD7746_CAPF_38P0 (1 << AD7746_CAPF_BIT_1) | (1 << AD7746_CAPF_BIT_0) #define AD7746_CAPF_62P0 (1 << AD7746_CAPF_BIT_2) #define AD7746_CAPF_77P0 (1 << AD7746_CAPF_BIT_2) | (1 << AD7746_CAPF_BIT_0) #define AD7746_CAPF_92P0 (1 << AD7746_CAPF_BIT_2) | (1 << AD7746_CAPF_BIT_1) #define AD7746_CAPF_109P6 (1 << AD7746_CAPF_BIT_2) | (1 << AD7746_CAPF_BIT_1) | (1 << AD7746_CAPF_BIT_0) #define AD7746_MD_IDLE 0 #define AD7746_MD_CONTINUOUS_CONVERSION (1 << AD7746_MD_BIT_0) #define AD7746_MD_SINGLE_CONVERSION (1 << AD7746_MD_BIT_1) #define AD7746_MD_POWER_DOWN (1 << AD7746_MD_BIT_1) | (1 << AD7746_MDF_BIT_0) #define AD7746_MD_OFFSET_CALIBRATION (1 << AD7746_MD_BIT_2) | (1 << AD7746_MD_BIT_0) #define AD7746_MD_GAIN_CALIBRATION (1 << AD7746_MD_BIT_2) | (1 << AD7746_MD_BIT_1) // Cap DAC A #define AD7746_DACAEN_BIT 7 #define AD7746_DACAEN (1 << AD7746_DACAEN_BIT) // Cap DAC B #define AD7746_DACBEN_BIT 7 #define AD7746_DACBEN (1 << AD7746_DACBEN_BIT) #define AD7746_DAC_COEFFICIENT 0.13385826771654F // 17pF/127 class AD7746 { public: AD7746(); AD7746(uint8_t address); void initialize(); bool testConnection(); void reset(); float getCapacitance(); //double CAPvalue(); void writeCapSetupRegister(uint8_t data); void writeVtSetupRegister(uint8_t data); void writeExcSetupRegister(uint8_t data); void writeConfigurationRegister(uint8_t data); void writeCapDacARegister(uint8_t data); void writeCapDacBRegister(uint8_t data); private: uint8_t devAddr; uint8_t buffer[19]; }; #endif /* _AD7746_H_ */
float AD7746::getCapacitance() { uint32_t capacitance; float capacitance1; I2Cdev::readBytes(devAddr,0x01,3,buffer); capacitance = ((uint32_t)buffer[1] << 16) | ((uint32_t)buffer[2] << 8) | (uint32_t)buffer[3]; // C=ieee_float(capacitance); capacitance1= (-0x80+(float)capacitance)*(4.096/8388608); return capacitance1; }
You might want to break things up into a couple of steps. Here's a similar function for an ADC that has an offset binary format:
I think you need to subtract the 0x800000 offset first, before casting as a float; you're doing this in a single step and I'm not sure what the result will be.
(Also it looks like you're subtracting 0x80, not 0x800000).
Try making a small test program that only exercises that formula, step through a range of input values, and make sure the output is as expected. That way you can debug this completely independently of the actual part.
-Mark