Post Go back to editing

CN0540 PMOD CONNECTOR BLOCK P8 pinout

Category: Hardware
Product Number: EVAL-CN0540-ARDZ

It looks to me like the schematic and the board silk screen disagree on the pins of P8:

 from 

 from   

Is this a difference in revisions? The physical board that I have says Rev-B, so I guess I'll believe the silkscreen. If there is a Rev-C, what other differences are there, and where can I find a schematic for the Rev-B that I have?

Parents Reply
  • Another strange thing about the PMOD connector markings is that pins 6 and 12 are labeled 3V3, but in fact they are connected to IOREF. Furthermore, by default there is no connection between IOREF and 3V3, so, if I'm using the board with the PMOD connector and without Arduino, I need to add a jumper between P2 pins 2 and 4 in order to power the dc-to-dc stages.

Children
No Data