Post Go back to editing

CN0540 Example Program Ported to STM32 NUCLEO-L496ZG: Getting Started, FAULT

Category: Hardware
Product Number: EVAL-CN0540-ARDZ
Software Version: 1:9dd7c64b4a64

I plugged a CN-0540 into a NUCLEO-L496ZG. I then ported the Example Program to STM32CubeIDE without Mbed: AD-CN0540_STM_NUCLEO-L496ZG. I connected a  Wilcoxon 786A general purpose accelerometer.

Now, I'm trying to run and debug the thing. I've connected a terminal, and I get this:

****************************************************************
* EVAL-CN0540-PMDZ Demonstration Program -- (mbed) *
* *
* This program demonstrates IEPE / ICP piezo accelerometer *
* interfacing and FFT measurements using AD7768-1 *
* Precision 24-bit sigma-delta AD converter *
* *
* Set the baud rate to 115200 select the newline terminator. *
****************************************************************


Command Summary:

1 - Set ADC power mode
2 - Set ADC MCLK divider
3 - Set ADC filter type
4 - Set ADC AIN and REF buffers
5 - Set ADC to default config
6 - Set ADC VCM output
7 - Read desired ADC register
8 - Read continuous ADC data
9 - Reset ADC
10 - ADC Power-down
11 - Set ADC GPIOs
12 - Read ADC [censored] status
13 - Set ADC Vref and MCLK
14 - Print ADC measured data
15 - Set ADC data output mode
16 - Set ADC diagnostic mode
17 - Do the FFT
18 - FFT settings
19 - Set ADC Gains, Offsets
20 - ADC Scratchpad Check
21 - Compenzate Piezo sensor offset
22 - Set DAC output

If I enter 12, I get this:

== [censored] STATUS REGISER
[censored] error: FAULT
ADC error: OK
Dig error: OK
Ext. clock: OK
Filter saturated: FAULT
Filter not settled: OK
SPI error: OK
POR Flag: OK

Makes sense; the FAULT LED is on. At one point, I was able to run choice 21 - Compenzate Piezo sensor offset, but now that just hangs. 

I have a feeling that I just don't know how to operate this thing (although my port has not been debugged yet, so that could be a problem too). Any suggestions on where to start?



Remove extraneous sentence
[edited by: CK3 at 6:10 AM (GMT -5) on 21 Nov 2022]
Parents
  • I did a 9  - Reset ADC,  1 - Soft reset - over SPI, and 5 - Set ADC to default config, and got ad77681 successfully initializedDefault ADC settings successfull. The FAULT light is still on. 

    I tried 21 - Compenzate Piezo sensor offset and it appeared to hang, but when I pressed the RESET button it ran successfully! Now, 12 - Read ADC *CENSORED* status returns

    == *CENSORED* STATUS REGISER
    *CENSORED* error: OK
    ADC error: OK
    Dig error: OK
    Ext. clock: OK
    Filter saturated: OK
    Filter not settled: OK
    SPI error: OK
    POR Flag: OK

    However, the FAULT LED is still on!

    I have taken some voltage measurements:

    Test Point Description
    TP5 27.77 Connects to the 28V rail before it's reduced to 26V.
    TP6 7.14 Connects to the 7V rail before it's reduced to 5V.
    TP7 5.00 Connects to the +VS supply of the reference buffer.
    P1 pin 2 12.49 VINP
    IOVDD 3.29
    P9 pin 6 3.30 IOREF
    P10 12.55 ADG5421F D1: Drain Terminal.
    R61 12.49, 12.50 ADG5421F S1 & S2, D2 (Not sure which order)
    C3 26.01 26V
    DS1 1.65 DS1: FAULT

    From the ADG5421F datasheet, "To activate the switches ... The input signal must be between VSS − VT and VDD + VT." I'm seeing 12.49V, which is between -0.7 and 26.7. Again from the ADG5421F datasheet, "The FF pin is an open-drain output that requires an external pull-up resistor. The output of the FF pin is high when both the Sx pins are within the normal operating range." Does that mean that the CN0540 FAULT light is normally on, and goes off to indicate a FAULT?

    So, maybe I've got it running OK. Now to try to collect some data and take an FFT.

  • Hi CK3,

    Yes, you got it right. 

    The CN0540 Fault light is normally on since it has an open-drain output which requires pull-up resistor which cause the LED to be "ON" by default and the digital output pulls low when a fault condition occurs on either of the Sx inputs.

    Regards,

    Michelle

Reply
  • Hi CK3,

    Yes, you got it right. 

    The CN0540 Fault light is normally on since it has an open-drain output which requires pull-up resistor which cause the LED to be "ON" by default and the digital output pulls low when a fault condition occurs on either of the Sx inputs.

    Regards,

    Michelle

Children
  • Great, thanks! I guess there is no relation between the FAULT light and faults reported by 12 - Read ADC [censored] status, correct? How can I clear all of the fault flags? For example, I have this condition:

    12
    == [censored] STATUS REGISER
    [censored] error: FAULT
    ADC error: OK
    Dig error: OK
    Ext. clock: OK
    Filter saturated: OK
    Filter not settled: OK
    SPI error: OK
    POR Flag: FAULT

    As far as I can tell, the POR Flag is just telling be that a reset has occurred. Well, yeah, I did the reset to try to clear the flags. Does it hurt anything having these FAULT flags set? 

  • Hi  

    You’re right: when you perform reset, the POR flag bit will be set to 1. The POR flag indicates that a reset or a temporary supply brown out occurred.  When performing the “12 - Read ADC master status” command after reset, the POR Flag will indicate a fault. To clear this, just perform another “12 - Read ADC master status” command.

    Just to add on your previous inquiries, the “Filter saturated: FAULT” indicates that the digital filter is clipped on either positive or negative ADC full scale. Check that differential voltage at the input of the ADC is within +/- 4.096V.

    Regarding the “21 - Compenzate Piezo sensor offset”, it takes some time to perform this command (around ~30 seconds for each compensation iteration). I would avoid typing in other commands during this phase. See screenshot.

    The only reason I could think of that will cause a true hang-up using this command is when the MCU did not receive the DRDY interrupt signal from the ADC, which is unlikely.

    On another note, the DC offset / bias voltage that DAC can compensate is only up to 13V. DC offset / bias voltage greater than 13V may result to “Filter saturated: FAULT. Check the voltage at P1 pin 2, this should be <13V. A successful “21 - Compenzate Piezo sensor offset” should have a final mean voltage close to 0V (i.e. “Final Mean Voltage: -0.000079”, see screenshot above)

    Regards,
    Malcolm

  • Thanks, Malcolm. I'm still struggling to capture some meaningful data.

    You’re right: when you perform reset, the POR flag bit will be set to 1. The POR flag indicates that a reset or a temporary supply brown out occurred.  When performing the “12 - Read ADC master status” command after reset, the POR Flag will indicate a fault. To clear this, just perform another “12 - Read ADC master status” command.

    Ah, that works!

    Just to add on your previous inquiries, the “Filter saturated: FAULT” indicates that the digital filter is clipped on either positive or negative ADC full scale. Check that differential voltage at the input of the ADC is within +/- 4.096V.

    Regarding the “21 - Compenzate Piezo sensor offset”,

    I'm having difficulties here. Once I got it to zero out perfectly, as measured at R22 & R23; ADA4945-1 +IN & -IN. But most of the time, it winds up way out. 

    On another note, the DC offset / bias voltage that DAC can compensate is only up to 13V. DC offset / bias voltage greater than 13V may result to “Filter saturated: FAULT. Check the voltage at P1 pin 2, this should be <13V. A successful “21 - Compenzate Piezo sensor offset” should have a final mean voltage close to 0V (i.e. “Final Mean Voltage: -0.000079”, see screenshot above)

    I see 12.5 V even at P1 pin 2 with the Wilcoxon 786A connected. In the Circuit Note, there are several measurements taken with "shorted inputs". I'm thinking I should get that configuration working right and connect the IEPE sensor later. However, I have questions about what "shorted inputs" really means. Just a jumper on P1? Maybe move the jumper from P10 to P1? Why is "inputs" plural?

    If I do move the jumper from P10 to P1 and run 21 - Compenzate Piezo sensor offset, I get this:

    21
    Initialize SAR loop (DAC MSB set to high)
    DAC code:8000 Mean Voltage: 0.010298
    UP

    SAR loop #: 15
    DAC code:c000 Mean Voltage: 0.000000
    DOWN

    SAR loop #: 14
    DAC code:a000 Mean Voltage: 0.000000
    DOWN

    SAR loop #: 13
    DAC code:9000 Mean Voltage: 0.050751
    UP

    SAR loop #: 12
    DAC code:9800 Mean Voltage: 0.000000
    DOWN

    SAR loop #: 11
    DAC code:9400 Mean Voltage: 0.048056
    UP

    SAR loop #: 10
    DAC code:9600 Mean Voltage: 0.000000
    DOWN

    SAR loop #: 9
    DAC code:9500 Mean Voltage: 0.047382
    UP

    SAR loop #: 8
    DAC code:9580 Mean Voltage: 0.000000
    DOWN

    SAR loop #: 7
    DAC code:9540 Mean Voltage: 0.000000
    DOWN

    SAR loop #: 6
    DAC code:9520 Mean Voltage: 0.012682
    UP

    SAR loop #: 5
    DAC code:9530 Mean Voltage: 0.070886
    UP

    SAR loop #: 4
    DAC code:9538 Mean Voltage: 0.047236
    UP

    SAR loop #: 3
    DAC code:953c Mean Voltage: 0.000000
    DOWN

    SAR loop #: 2
    DAC code:953a Mean Voltage: 0.000000
    DOWN

    SAR loop #: 1
    DAC code:9539 Mean Voltage: 0.012551

    Final DAC code set to:0 Final Mean Voltage: 0.000000

    Offset compenzation done!

    Now, if I do 12 - Read ADC [censored] status, I get this:

    12
    == [censored] STATUS REGISER
    [censored] error: FAULT
    ADC error: OK
    Dig error: OK
    Ext. clock: OK
    Filter saturated: FAULT
    Filter not settled: OK
    SPI error: OK
    POR Flag: FAULT

    P7, SHIFT, is 35.1 mV.

    R22 (ADA4945-1 [FDA] +IN) is 1.81 V, R23 (-IN) is 1.39 V, difference is 0.424 V. 

    R64 to R65 (FDA_OUT_N & FDA_OUT_P) is 4.96 V.

    C9 (AD7768-1 AIN+ & AIN-) also measures 4.96 V; clearly outside the range of -4.096 - +4.096, which explains the Filter saturated: FAULT, right?

  • I am making some great progress. The breakthrough came when I realized that the SHUTDOWN signal is active low, which was not obvious to me until I studied the schematic. I had been running with the DAC buffer disabled!

    Regarding the “21 - Compenzate Piezo sensor offset”, it takes some time to perform this command (around ~30 seconds for each compensation iteration). I

    You're not kidding. I thought I still had a hang, and was trying various things until I got distracted while it was running and came back a while later to find that it had run to completion!

    As a sort of verification test, I connected a 1 kΩ resistor across P1 (GND and VIN) and did 17 - Do the FFT, which yielded:

    THD:-2.038 dB
    SNR:-7.394 dB
    DR:104.990 dB
    Fundamental:-117.300 dBFS
    Fundamental:148.438 Hz
    RMS noise:25.390626 uV
    LSB noise:52.000

    12 - Read ADC [censored] status reports no FAULTs. Then, I did 18 - FFT settings, 3 - Print FFT plot, and then graphed the results:

    This seems to accord well with Figure 10. FFT for the DC-Coupled Solution with Shorted Input, DAC Output
    at Half Scale in the Circuit Note.

    Now, I think I'm ready to connect the Wilcoxon IEPE sensor.

  • Hi  

    Great to hear that you were able to make the circuit work.
    Having it in "shutdown" affects "DAC_BUF_EN" and "SW_IN" nodes, which affects a lot of sub-blocks in the circuit, including the ADA4807 amplifiers. A disabled amplifier can rail to either supply voltage, making it very unpredictable. 

    To be clear, "shorted inputs" in this circuit means shorting the VINP input node to ground.
    Like what you were saying, having a jumper across P1 would achieve this, ideally having VINP=0V.

    I believe that 12.5V is the DC bias of the sensor, which can be compensated by the DAC. I hope you are able to get a sensible output from the accelerometer!

    Regards,
    Malcolm

  • I believe that 12.5V is the DC bias of the sensor, which can be compensated by the DAC. 

    With the sensor connected I see:

    VIN (P1): 12.49 V

    SHIFT (P7): 4.68 V

    I hope you are able to get a sensible output from the accelerometer!

    It looks good so far. FFT with the 786A just lying on the bench:


    THD: -1.475 dB
    SNR: -1.380 dB
    DR: 98.336 dB
    Fundamental: -102.672 dBFS
    Fundamental: 179.688 Hz
    RMS noise: 83.984378 uV
    LSB noise: 172.000

    I (loosely) attached a vibrator and got this:

    THD: -7.439 dB
    SNR: -4.976 dB
    DR: 51.531 dB
    Fundamental: -56.702 dBFS
    Fundamental: 1210.938 Hz
    RMS noise: 9252.442047 uV
    LSB noise: 18949.000

    No FAULTs are reported in the [censored] Status Register.