Post Go back to editing

CN0429 terminal output question

Category: Software
Product Number: CN0429

Hi,

I have similar strange data format problem exported from CNO429 board.

-------------

runeis
EIS test started. Depending on the frequency range,
this can take several minutes. Don't enter additional
commands until the test is finished.
Test finished! Results ready.
readeis
------------------

Frequency, Magnitude, Phase, Real Mag, Imag Mag
1000.000000, 39706.496094, 63.206104, 5000.000000, 8527.833008
63.456184, 10000.000000, 4308.209473, 55.793385, 20000.000000
2160.175293, 42.652138, 30000.000000, 1440.804688, 30.614855
40000.000000, 1089.133545, 18.356434, 50000.000000, 925.604431
5.838364, 60000.000000, 908.778748, 5.597518, 70000.000000
906.025513, 5.493637, 90000.000000, 873.918823, 4.816417
160000.000000, 887.299622, 5.532125, 200000.000000, 897.069336
5.868478, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000
-680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000
-680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000
-680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000
-680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000

-----------
The addtional headers with Real Mag and Imag Mag in the data set are not supplied by the board. Thous are 2 extra epmpty columns make the exported data to shift around. We have 5 headers but only 3 of them are exported. So, the frequeny, magnitude and phase columns are not correct since frequency data was shifted 2 empty columns each time. Some body expert on the hex file debuging proceedure can help us to erase those headers from 'readeis' command. That might solve format issue I guess. There are also very large numbers that I can not understand. What is the meaning of them?

The same problem appears on the 'readeisfull'. There are 15 headers but only 13 data colums are exported. So, 2 unsupported headers should be erased from the Prebuilt CN0429 Hex File

---------------

readeisfull

---------------
Frequency, Rload+Rsens_real, Rload+Rsens_img, Rload_real, Rload_imag, Rcal_real, Rcal_imag, Mag_Rsens+Rload, Mag_Rload, Mag_Rcal, Mag_Rsens, MAG, PHASE, Real_Mag, Imag_Mag
1000.000000, -102, -65, 4130, -42367, 2333, -23930, 120.950401, 42567.824219, 24043.457031, 42513.164062, 39706.496094, 63.206104, 5000.000000, -680551753099730589857677888622713372672.000000
-680546155154679981996640879181358432256.000000, 19821, -37519, 11192, -21192, 1141616089, 1193656540, 23965.845703, 42180.296875, 8527.833008, 63.456184, 51.061523, 0.000000, -680520721013037002801929249328245768192.000000, 0.000000
-679604442876782434938857008304148709376.000000, 19595, -13378, 1149740673, 1193547255, 1186552960, 1193388698, 4308.209473, 55.793385, 64.473633, 0.000000, 20000.000000, 0.000000, 0.000000, 0.000000
0.000000, 1157483958, 1193122558, 1186071849, 1192734467, 1158087374, 1110088650, 84.334229, 0.000000, 30000.000000, 0.000000, 0.000000, 0.000000, 0.000000, 2767.431396
37711.203125, 1185308523, 1191831685, 1152653760, 1106570041, 1120169968, 0, 40000.000000, -680506888409687312362700117302868705280.000000, 0.000000, -679618518869047369198131227696541204480.000000, 0.000000, -680031225339662473387917706365709058048.00000
31193.386719, 1149772870, 1100143098, 1121408448, 0, 1195593728, -3287, -680556864266950710078624723330037448704.000000, -679350912756736789058557667663073509376.000000, -680379677136653209085801120142802812928.000000, -67987926952691191507310149355907422
5.838364, 1122025432, 0, 1198153728, -1459, -2469, -11167, -679614908600137919200795765085812293632.000000, -680307958536294696779182042662255460352.000000, -680029115969063693614193615851575312384.000000, 2867.863770, 25941.550781, 14642.899414, 5.597518
0.000000, 1200142336, 1022, -2157, 10883, -18584, 6118, -680138722110561827241164626797524942848.000000, 2386.866699, 21536.126953, 12154.090820, 19159.480469, 906.025513, 0.000000, 90000.000000
-680429571864278192195044030380966412288.000000, 2557, -30732, 20050, -17324, 11359, 1166229619, 36694.117188, 20715.882812, 32507.923828, 873.918823, 4.816417, 112.538513, 0.000000, -680489364407789757319453826877757587456.000000
0.000000, -14459, 12937, -8216, 1161797985, 1188307415, 1181709746, 24100.646484, 887.299622, 5.532125, 112.373840, 0.000000, 200000.000000, 0.000000, 0.000000
0.000000, 11353, 1159100213, 1185429954, 1178457734, 1184203682, 1147159664, 5.868478, 112.266541, 0.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000,
-680564693277057719623408366969033850880.000000, -1, -1, -1, -1, -1, -1, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -680564693277057719623408366969033850880.000000, -6805646932770577196234083669690338

----------------------

Is there any body to help us to erase those unsupported headers and replace the Prebuilt CN0429 Hex File ?

Thanks in advance.

Salih Okur

Edit Notes

split this question out from an older post, renamed the post
[edited by: Brandon at 2:11 PM (GMT -4) on 8 Sep 2022]