Hello Everyone,
I recently bought the evaluation board CN-0510. As I tried to to connect the board with SensorPal,
the following message came on the prompt "Error in opening connection. Invalid response from firmware"
The board is recognized by the PC, And the Switch Configuration for the data transfer(S2) is configured on the "USB".
One thing I also noticed is that the LED "DS3" keeps blinking in a frequency of around 1 Hz. Since I cannot access the datasheet of the EVAL-ADICUP3029, I cannot debug which signal is that.
Has someone encountered this error?
Best Regards
PMarq