Hello,
I am new to the world of interfacing with electrochemical sensors, and, a relatively new EE as well. I was hoping we could go through some of the design details in the diagram below.
- U2-A
- I don't understand the feedback network, the inner loop with C3 looks like an integrator, but, with the resistors seems to form an RC low pass. Could you describe the how/why of the feedback network?
- Also, why there are two RC stages using the same values?
- What are the reasons R3, R4, R5, and R6 being the same values?
- I don't understand the feedback network, the inner loop with C3 looks like an integrator, but, with the resistors seems to form an RC low pass. Could you describe the how/why of the feedback network?
- Is Vref in this circuit an external supply?
- When I read about these circuits virtual ground is mentioned quite a bit; here, 1.2V (generated from U4) is serving as the virtual ground with VREF super-imposed?
- U5
- This is serving as an ADC Buffer to ensure the input capacitor on the ADC input isn't loaded down?
Thanks for your help!