I'm looking at ordering gas sensors the EVAL-CN0429-EBZ. The BOM parts list doesn't seem to be consistent with the photos online. All the photos of the PCB have gold inserts mounted on the board for the gas sensor to allow for easy insertion and removal. I cannot find these parts listed on the BOM, instead there seems to be two different options;
| 10 | 1 | E026504 | MOD CARBON MONOXIDE SENSOR | 110-102 | M110-102 | N/A | N/A | N/A | M1 | SPEC SENSORS | 110-102 |
| 12 | 2 | E023091 | CONN-PCB HDR SIL VERT, 2.0MM PITCH | M22-2010205 | CNHDR1X2H207 | N/A | N/A | N/A | P2,P3 | HARWIN | M22-2010205 |
I think the BOM is for a SPEC SENSOR 110-102?
Please advise.
AFisher