CN-0267: FAQ

  • Created
  • Updated
Was this helpful?
  • CN-0267 - Evaluation of the board

    Q Do I need a HART source to evaluate the board? A Yes, in order to evaluate the HART protocol you will need to have access to a HART source.
  • CN-0267 - HART stack

    Q Do you provide a HART stack? A No we do not provide a HART stack, we can only implement command 0 which is a simple command that confirms the presence of working HART device. Customers…
  • CN-0267 - JLink adaptor

    Q I have an older 20 pin JLink adaptor, can I use it? A The development kit for our ARM based products has been updated and now includes all you need on one board connected to the PC by USB…
  • CN-0267 - missing software download area on ftp site

    Q I purchased CN-0267 kit. The documentation that we received with the CN-0267 board mentions we should download 'Software for CN0267 Evaluation Board' from ftp://ftp.analog.com/pub/cftl/CN0267…
  • CN-0267 - Sensor recommendation

    Q What pressure sensor do you recommend for use with the HART enabled Field Instrument reference circuit in CN-0267? A We have not included a sensor with the board enabling you to quickly connect…
  • What do I need if I want to do further development with the ADuCM360 and CN-0267 reference design?

    Q What do I need if I want to do further development with the ADuCM360 and CN-0267 reference design? A If you want to do additional development work you will need a Cortex M3 core development Kit…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.