Hello,
We are evaluating the AD3552R DAC using the EVAL-AD3552RFMC1Z and SPD-H1.
I downloaded and installed the latest ACE software (1.24.3098.1398) and connected the boards.
ACE software is able to recognize the connected devices and I can fully navigate the menus without errors.
However, I am not able to get the board to output the waveforms when I follow the waveform generation guide.
The 1kHz 'DefaultSingleTone' vector is added to the DAC and 'Play' is clicked, then the ACE software indicates that there is a "Transaction Error".

No further information is provided by the ACE software. Please help troubleshooting this issue.
Error log from the software is attached here, Error.zip