Post Go back to editing

AD7626 signal chain for higher frequency measurements >1MHz

 I have used the AD7626 in previous designs and I am considering it for a higher frequency measurement design - is there performance for the AD7626 with input frequencies > 1 MHz and can you recommend an ADC driver to maximize performance?



.
[edited by: EstiS at 7:59 AM (GMT -4) on 20 May 2021]
Parents
  • The AD7626 datasheet does show AC dynamic performance with input frequencies up to 2.4MHz. In addition there is a Circuit Note CN0105 that shows the AD7626 10 MSPS 16 bit ADC used with the ADA4932-1 Fully Differential Amp doing Single ended to differential conversion in addition to driving the AD7626 input. This Circuit note shows performance with a tone of 2.4MHz the SINAD is >84.5 dB. Also use the Precision ADC Driver tool to test the AD7626 with different ADC driver options at higher input frequency tones to understand the best option for your design.

Reply
  • The AD7626 datasheet does show AC dynamic performance with input frequencies up to 2.4MHz. In addition there is a Circuit Note CN0105 that shows the AD7626 10 MSPS 16 bit ADC used with the ADA4932-1 Fully Differential Amp doing Single ended to differential conversion in addition to driving the AD7626 input. This Circuit note shows performance with a tone of 2.4MHz the SINAD is >84.5 dB. Also use the Precision ADC Driver tool to test the AD7626 with different ADC driver options at higher input frequency tones to understand the best option for your design.

Children
No Data