A passive RC circuit has a real pole or zero only, and its pole or zero is on the real axis of the complex s-plane. Using active feedback shifts a real pole from the real-axis to two points, one between negative real axis and positive j-axis and one between negative real-axis and negative j-axis (the left plane region) thus generating a complex pole pair.
For example, a passive RC, second order real pole, lowpass filter can be transformed by feedback into an active RC, second order, complex pole pair lowpass filter.