Post Go back to editing

Do I need a reference buffer to drive an ADC?

Thread Summary

The user asks if a reference buffer is needed to drive an ADC. The final answer explains that most references require a buffer to provide a low-impedance output, improving load regulation and handling medium-frequency transients. Some reference ICs have an integrated buffer, but it may not be sufficient for all ADCs. The AD4134 is an example of an ADC that can be driven directly by a reference or a reference with an integrated buffer, as per the datasheet recommendations. The accompanying answer suggests a webinar for a more detailed discussion on driving ADC reference inputs.
AI Generated Content

Do I need a reference buffer to drive an ADC?

Parents
  • Most references will need a reference buffer to drive an ADC. The reference buffer provides a low-impedance output that improves load regulation (the change in output voltage with load current). A reference buffer will also assist in medium-frequency transient load demands. High-frequency load transients can generally only be supplied with large external capacitors.

    Some reference ICs include an integrated buffer. This buffer is a general-purpose buffer and may not be adequate to drive a specific ADC.

    Some ADCs, have internal buffering or features that may allow them to be driven directly by a reference or a reference with an integrated buffer (e.g. AD4134). Usually the ADC datasheet will give recommended connections and suggested components for the reference inputs.

Reply
  • Most references will need a reference buffer to drive an ADC. The reference buffer provides a low-impedance output that improves load regulation (the change in output voltage with load current). A reference buffer will also assist in medium-frequency transient load demands. High-frequency load transients can generally only be supplied with large external capacitors.

    Some reference ICs include an integrated buffer. This buffer is a general-purpose buffer and may not be adequate to drive a specific ADC.

    Some ADCs, have internal buffering or features that may allow them to be driven directly by a reference or a reference with an integrated buffer (e.g. AD4134). Usually the ADC datasheet will give recommended connections and suggested components for the reference inputs.

Children
No Data