My noise simulation result with AD8237 in LTspice does not align with the datasheet spec, does anyone else have this issue?
AD8237
Recommended for New Designs
The AD8237 is a micropower, zero drift, rail-to-rail input and output instrumentation amplifier. The relative match of two resistors sets any gain from...
Datasheet
AD8237 on Analog.com
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
My noise simulation result with AD8237 in LTspice does not align with the datasheet spec, does anyone else have this issue?
Different parameters can change the outcome of a noise simulation.
The first step is to check if some gain is implemented. When using the AD8237 with some gain, the noise output will not correspond to the datasheet specifications. To get the datasheet value back, you need to divide the obtained value by the gain used. For example, if a gain of 100 is implemented, then the noise output will print a value around:
The second origin of noise difference is to check if parallel components are introducing some noise. The “noiseless” command can be added for resistors to remove any noise coming from those component.
Check out this video LTspice IV: Noise Simulations - YouTube to learn more about Noise simulation!
Different parameters can change the outcome of a noise simulation.
The first step is to check if some gain is implemented. When using the AD8237 with some gain, the noise output will not correspond to the datasheet specifications. To get the datasheet value back, you need to divide the obtained value by the gain used. For example, if a gain of 100 is implemented, then the noise output will print a value around:
The second origin of noise difference is to check if parallel components are introducing some noise. The “noiseless” command can be added for resistors to remove any noise coming from those component.
Check out this video LTspice IV: Noise Simulations - YouTube to learn more about Noise simulation!