How do I know that I'm biasing the AD8235/AD8237 correctly?
Edit Notes
.[edited by: ESanz at 7:32 AM (GMT -4) on 28 Sep 2021]
AD8237
Recommended for New Designs
The AD8237 is a micropower, zero drift, rail-to-rail input and output instrumentation amplifier. The relative match of two resistors sets any gain from...
Datasheet
AD8237 on Analog.com
AD8235
Production
The AD8235 is the smallest and lowest power instrumentation
amplifier in the industry. It is available in a 1.5 mm × 2.2 mm
wafer level chip scale package...
Datasheet
AD8235 on Analog.com
How do I know that I'm biasing the AD8235/AD8237 correctly?
The AD8235 and AD8237 are instrumentation amplifiers (in-amps) and these low power devices are great for a breadth of different applications that include pressure, strain or even temperature sensing.
The AD8235 and AD8237 just like many in-amps have a reference input pin that can be used to apply a bias voltage to set the output of the in-amp to the correct level for the downstream circuitry. The ability to adjust the output of the in-amp will ensure the complete output signal swing is use. For 3 op-amp in-amps and 2 op-amp in-amps like the AD8235, internal nodes can saturate if not biased correctly. When configuring the in-amp for your design it is important to note that the output signal of the in-amp is dependent on the input signal, reference voltage, the gain as well as the power supply voltage and is typically characterized by the "Diamond Plot".
The AD8237 is an indirect current mode in-amp and has built in capability to eliminate the Diamond Plot making it much easier to bias.
As part of the precision studio toolkit from analog devices, you will find the Instrumentation Amplifier Diamond Plot Tool (link here) There is an excellent article in analog dialogue that unveils the secrets of the diamond plot tool found here, so have a read before diving into your design as it highlights some of the key considerations when configuring the in-amp in your design. The tools supports all of ADIs instrumentation amplifiers, so you will find both the AD8235 and AD8237 supported as well as many of our other instrumentation amplifiers.
The AD8235 and AD8237 are instrumentation amplifiers (in-amps) and these low power devices are great for a breadth of different applications that include pressure, strain or even temperature sensing.
The AD8235 and AD8237 just like many in-amps have a reference input pin that can be used to apply a bias voltage to set the output of the in-amp to the correct level for the downstream circuitry. The ability to adjust the output of the in-amp will ensure the complete output signal swing is use. For 3 op-amp in-amps and 2 op-amp in-amps like the AD8235, internal nodes can saturate if not biased correctly. When configuring the in-amp for your design it is important to note that the output signal of the in-amp is dependent on the input signal, reference voltage, the gain as well as the power supply voltage and is typically characterized by the "Diamond Plot".
The AD8237 is an indirect current mode in-amp and has built in capability to eliminate the Diamond Plot making it much easier to bias.
As part of the precision studio toolkit from analog devices, you will find the Instrumentation Amplifier Diamond Plot Tool (link here) There is an excellent article in analog dialogue that unveils the secrets of the diamond plot tool found here, so have a read before diving into your design as it highlights some of the key considerations when configuring the in-amp in your design. The tools supports all of ADIs instrumentation amplifiers, so you will find both the AD8235 and AD8237 supported as well as many of our other instrumentation amplifiers.