Post Go back to editing

Right leg drive - Meaning & Implementation

Thread Summary

The user asked about the right leg drive (RLD) technique and its implementation with the AD8233. The final answer explains that RLD reduces common mode interference by driving an opposing signal into the patient, improving the common mode rejection ratio (CMRR). The AD8233 has an integrated RLD amplifier, and the EVAL-AD8233 customer evaluation board demonstrates this functionality, with detailed implementation information available in the user guide.
AI Generated Content
  • Right leg drive (RLD) is a technique that uses an amplifier to reduce common mode interference when making bipotential measurements. There are many different types of signals that can be easily picked up by not just the human body but also the electrodes and cables. An example of such interference could be 50Hz/60Hz noise signals from the mains. Therefore when selecting an instrumentation amplifier for Biosignal measurements such as ECG or EMG it's important to select a device that has high common mode rejection ratio (CMRR). Take a look at this post on Engineer Zone for a little more insight on how this right leg drive technique works.  

    The AD8233 has an integrated RLD amplifier that senses the common mode voltage present at the input signal and can drive an opposing signal into the patient that is being monitored. Thus the driven electrode functionality maintains a constant voltage between the patient and the AD8233 greatly improving the common mode rejection ratio. The AD8233 customer evaluation board EVAL-AD8233 implements this and key information on the implementation can be found in the user guide for the AD8233  

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.