Engineers developing sensor solutions for the intelligent edge are continually pressured to reduce system size and cost. Analog Devices’ Easy Drive SAR ADCs use innovative input architectures to reduce ADC-driver requirements, simplifying the analog front end. Often, this leads to either a cost reduction, reduced solution size, power savings, or all three, without sacrificing performance.
A conventional signal chain construction uses an input stage for gain followed by a driver stage for the ADC.

Figure 1. Traditional sensor signal chain.
This signal chain utilizes a low bandwidth first stage to provide gain, and a high bandwidth driver stage.
Why is the high bandwidth driver needed?
SAR ADCs work by charging a sampling capacitor to the input voltage during each sampling period. The sampling capacitor will be charged or discharged at the start of each acquisition phase, causing voltage transients on the ADC input at the beginning of the sample acquisition phase. The ADC driver must have sufficient bandwidth and current drive to settle these transients before the start of the conversion phase, otherwise, distortion is introduced into the sampled signal. An example is shown below.
This signal chain, with a traditional SAR ADC input, would exhibit an input transient as shown in the next figure.

Figure 2. Transient response with wide bandwidth ADC driver.
Assuming a 3.3 V reference, 16-bits of resolution, and a 1 MSPS sample rate, the ADC input has settled to less than ½ LSB of error at the start of conversion, an acceptable error limit for a precision signal chain.
If the driver stage is eliminated, and the gain stage is used to drive the ADC, the solution can be more compact, lower power, and cheaper.

Figure 3. Signal chain without dedicated ADC driver.
However, if a traditional SAR ADC is used, the transient response won’t be settled using the lower bandwidth driver. The following figure illustrates this case, where the transient response is still settling at the start of conversion, inducing a 15-millivolt error in the sample value (~603 LSBs). Disregarding other error sources in the circuit, this is nearly 0.5% error due to the ADC alone.

Figure 4. Unsettled transient without dedicated ADC driver
One of the several innovations employed by ADI’s Easy Drive ADCs is to use extremely small sampling capacitance. By using a reduced sampling capacitor value, less charge is required. This eases the requirements for the ADC driver, meaning that an op amp with lower bandwidth and lower current drive can be used. In op amps, wider bandwidths usually equate to higher power, and vice versa. By reducing the required bandwidth, it’s possible to use a lower power driver and in some cases, eliminate the driver altogether.
Using a 16-bit Easy Drive ADC under the same operating conditions, the transient would appear as in the next plot:

Figure 5. Easy Drive ADC transient response with low bandwidth driver.
Comparing the plots, we see that the Easy Drive ADC transient settles more quickly and to within ½ LSB error. In this example, by eliminating the driver stage, cost, solution size and power have been improved.
To learn more about Easy Drive circuit design techniques, see the following references.
- Tech Note: Can Analog Devices' Easy Drive ADCs simplify multi-channel sensor signal chain design?
- Tech Note: Can Analog Devices' Easy Drive ADCs help achieve precision signal measurements?
- Video: Analog Devices EasyDrive︎ ADCs
- Blog: LTspice®︎ and EasyDrive︎ — A One-Two-Punch for Design Efficiency
- Tech Note: Easy Drive in SAR ADCs - Signal chain design advantages
|
Featured Products |
|
![]() |
AD4052: Compact, Low Power, 16-Bit, 2 MSPS/500 kSPS Easy Drive SAR ADC |
![]() |
AD4691: 16-Channel, Easy Drive Multiplexed SAR ADC with Averaging Filters Per Channel |
![]() |
AD4060: Compact, Low Power, 12-Bit, Easy Drive SAR ADC with I3C Interface |
Explore and compare the full offering of Easy Drive ADCs from the Analog Devices Product Selection Table.