Post Go back to editing

Less decoupling in gate drivers

Can I get away with less decoupling in the gate drivers?



.
[edited by: EstiS at 2:04 PM (GMT -4) on 19 May 2021]
  • It is possible to use less than the recommended 0.1 µF + 10 µF capacitance on the output supply,, however it should be noted that using smaller decoupling capacitors can lead to higher voltage droop during turn on edges.

    It is recommended that the full 10 µF decoupling is used for best performance