Do I have to connect the Miller clamp on the ADuM4121?
.
[edited by: EstiS at 2:00 PM (GMT -4) on 19 May 2021]
Do I have to connect the Miller clamp on the ADuM4121?
No, If the Miller clamp is not being used, it is recommended to short it to GND2.
However it should be noted that the ADuM4120 has similar performance to the ADuM4121 and has a smaller package so could be used in place.