Post Go back to editing

Best slew rate/settling time currently achievable

What is the best slew rate/settling time achieved in the currently available High Voltage Precision Signal Chain solutions?



.
[edited by: ESanz at 10:23 AM (GMT -4) on 27 Sep 2021]
Parents
  • Many precision DAC's like AD5504 and AD5535B are tuned for high DC performance, not for settling time. The precision high voltage DAC slew rates are less than 10V/us, with settling times typically about 60us.  The high-speed current drive amp, ADA4870, supports 2500V/us typ with 82ns typ settling time. 

Reply
  • Many precision DAC's like AD5504 and AD5535B are tuned for high DC performance, not for settling time. The precision high voltage DAC slew rates are less than 10V/us, with settling times typically about 60us.  The high-speed current drive amp, ADA4870, supports 2500V/us typ with 82ns typ settling time. 

Children
No Data