Analog.com
Analog
Dialogue
Wiki
English
Analog.com
Analog
Dialogue
Wiki
简体中文
EngineerZone
Site
Search
User
Site
Search
User
EngineerZone
Search
Log in
Site
Search
Log in
Home
Blogs ⌵
EngineerZone Spotlight
The Engineering Mind
Browse ⌵
All Groups
All Members
Support ⌵
3D ToF Depth Sensing
Amplifiers
Analog Microcontrollers
Audio
Clock and Timing
Data Converters
Design Tools and Calculators
Direct Digital Synthesis (DDS)
Embedded Vision Sensing
Energy Monitoring and Metering
FPGA Reference Designs
Industrial Ethernet
Interface and Isolation
Low Power RF Transceivers
MEMS Inertial Sensors
Motor Control Hardware Platforms
Optical Sensing
Power By Linear
Processors and DSP
Reference Circuits
RF and Microwave
Switches/Multiplexers
Temperature Sensors
Video
Wide Band RF Transceivers
Wireless Sensor Networks Reference Library
My EZ
More
Cancel
主页
浏览 ⌵
收件箱
个人设置
会员
专区列表
论坛专区 ⌵
放大器专区
精密转换器专区
音频专区
ADE电能计量专区
MEMS和传感器专区
接口和隔离专区
Power 中文专区
ADUC微处理器专区
锁相环专区
开关和多路复用器专区
温度传感器
基准电压源专区
资源库
论坛使用指南
技术支持参考库
在线研讨会
论坛社群活动
论坛激励活动
More
Cancel
Power By Linear
Documents
ADM1062: Data storage on EEPROM
Q&A
Discussions
Documents
File Uploads
Video/Images
Tags
Managers
More
Cancel
New
Power By Linear requires membership for participation - click to join
+
Documents
1/f noise of the ADM7150/ADM7151 be reduced?
ADIsimPE Powering Dual Supplies Precision ADCs
ADIsimPE support
ADIsimPower Design Tools Download
ADIsimPower user guide 832
ADIsimPower user guide 842
Adjustable vs. fixed voltage option
ADM1030: Lowest pull resistor
ADM1030: Lowest pull up resistor
ADM1031: Unused D+ and D+ pins
ADM1060 Power Sequencer support for USB interface
ADM1062: ADC readback mode
ADM1062: Data storage on EEPROM
ADM1066 AUX Signals in the State Machine
ADM1066: application questions
ADM1068: internal Reference maximum current
ADM1085: transistor count
ADM1166 - CRC, configuration, EEPROM and RAM at startup query
ADM1166 Sequencing differential voltage query (SR#: 1239446)
ADM1171: Current limit device
ADM1175_Vbus spec
ADM1232: Spikes on VCC
ADM1816: Voltage on reset line does not go to zero until the supply is approx 1V
ADM2483_ESD AB impedance
ADM2483_PV pin function
ADM2484 revA board
ADM2484E voltage specification
ADM2485 VDD2 voltage
ADM2587 layout to pass EMI/EMC tests
ADM2587E isolation ratings
ADM2587E max allowable voltages on RS485 pins
ADM2587E power consumption
ADM2587E Power consumption (1)
ADM2682E start up currents
ADM2682E/ADM2687E Creepage and Clearance
ADM2682E/ADM2687E Isolation Voltage
ADM2682E/ADM2687E providing additional current to external devices
ADM2682E/ADM2687E Recommended Application Notes
ADM2687E: Minimum and Maximum Viso specifications
ADM2687E: Power consumption while dissabled
ADM3053 max current on Visoout
ADM3053 Round Trip Propogation Delay
ADM3053 stitching capacitance
ADM3053/3053/3054 Isolated CAN Transceiver
ADM305x differences
ADM3075EARZ: What's its impedance when no supply is applied?
ADM3202 alternatve with swapped CMOS/RS-232 pins?
ADM3251 heat generation
ADM3251E - Prevent - minimize EMI isses
ADM3251E: Gerber file EVAL-ADM3251EEBZ
ADM3251_application high working temperature
ADM3252: Detecting the cable connection
ADM3491: Is resistor Rt needed between Y and Z (transmitter side) or only on the receiver side?
ADM4073T: Settling Time
ADM483E: Operation in fail safe mode
ADM485 - how does the fail-safe feature mentioned in the datasheet work
ADM6320CX and WDI query/comments(SR#: 1200246)
ADM696: Datasheet reset assertion guarantee
ADM706: IBIS model
ADM706: what happens if WDI Pin is left open or "High Impedance"
ADM706: What is the difference between difference ADM706PARZ and ADM706RARZ?
ADM709RAR_theta JA & theta JC
ADM7154, ADM7155: Are there any other design considerations for low noise?
ADM7154, ADM7155: Is the soft start time programmable?
ADM7154, ADM7155: What is the recommended headroom voltage?
ADM869L: absolute maximum ratings
ADP-I2C-USB _USB to I2C Interface Connector
ADP1046 Daughter Board compatible with existing one for ADP1043
ADP1048 - is is possible to use the ADP1048 with higher input frequencies?
ADP1048: Which control mode is used: continous current or discontinuous current?
ADP1051: EEPROM programming procedure
ADP125 and ESR values
ADP130: Does the datasheet undervoltage lockout spec apply to Vin or Vbias?
ADP160-IGND Max
ADP1607 reverse current protection with EN high/low
ADP1607 to supply ADAU1761
ADP1621 and ADP2300/01: positive to negative conversion
ADP1829 Dual buck controller with a high side N channel FET
ADP197:
ADP198 What happens when Vout > Vin ?
ADP2108 layout considerations (high frequency switching regulator layout considerations)
ADP2118: fixed Output FB Pin
ADP2384, ADP2386 - Benefits of hiccup mode during over current/short circuit
ADP2384, ADP2386 - Deglitch time when PGOOD reversing
ADP2384, ADP2386 - Fastest soft start time
ADP2384, ADP2386 - Leaving RT pin open
ADP2384, ADP2386 - PGOOD feature
ADP2384, ADP2386 - PGOOD pin open
ADP2384, ADP2386 - Programming soft start time
ADP2384, ADP2386 - Setting the switching frequency
ADP2384, ADP2386 - SS pin unconnected
ADP2384, ADP2386 - Treatment of GND-EP (pin 25) and SW-EP (pin 26)
ADP2384, ADP2386 - Use of EN threshold to set input voltage UVLO
ADP2386, ADP2384 - Support of pre-charge start up
ADP2441 External Diode between SW and PGND
ADP2441 Floating Pins
ADP2441 Minimum ON Time
ADP2441 Peak Current Limit
ADP2441 Precharge Startup
ADP2441 VCC Pin
ADP2441: Factors to Improve Efficiency
ADP2441ACPZ-R7 Power Dissipation
ADP2504 Issues with supplied current and current limiting
ADP3040 - information available?
ADP3302: Input protection
ADP3330: max reverse voltage
ADP3330: Reverse current
ADP3338: Thermal and overcurrent protections
ADP5046 shuts down
ADP5050 considerations for simulations under Simplis
ADP5050 Pin20 as address pin
ADP5061 reading via I2C
ADP5090_91: Need to cut the load of ADP5090 if temperature is under 0�C and above 40�C for Li-Ion Battery Charging
ADP5585 interrupt (/INT pin) not asserting
ADP5588_work under 3.3V
ADP7112: Materials declaration is missing from ADP7112 web page
ADR01 reference's output long-term drift calculation
ADR125: Output Capacitance
ADR127: Turn-on time when using a 0.1uF in parallel with a 10uF at its output?
ADR3450
ADR365 supplied with DCDC converter
ADR366: External Capacitors
ADR381 output capacitor ESR
any isolated RS-422 driver with no bit errors during EFT test?
Are any external components required?
Are there any layout considerations when designing in the ADP5052?
Are these devices automotive replacements for the ADM6316/18/19/20/21/22 parts?
Boost converter recommendation
CAN FD version of ADM3053
Can I configure ADM3491 in half duplex mode of operation
Can the 4 bucks run at different frequency?
Can the ADP1047/8 be used as a three-phase PFC controller?
Can the ADP1051 be used to control a buck fed push pull (or full bridge) power stage?
Can the CS1 pin of the ADP1043A, ADP1046A, ADP1050, ADP1051, ADP1055 be floating?
Can the voltage VS- pin (VS3- for ADP1046A) of ADP1050/51/55 operate at a voltage higher than 0.3V?
Can you supply PVIN1, PVIN2, PVIN3, PVIN4 and PVIN5 independently?
Can you use an inductor not specified in the datasheet?
Customer programmable fuses on ADP5053?
DAC power up default state of ADM1066
Difference between ADM2682E and ADM2687E
Does the output noise of the ADM7154/ADM7155 scale with the output voltage?
Drivers for Linux, No-OS microcontrollers and FPGA
Emissions by ADM2582E at 1.5GHz .. 1.1GHz
Explanation on ADM3483 Driver Output/Receiver Input Voltage
FAQ: Can I use the square wave at 50% duty cycle to sync with the ADP1047/48?
FAQ: How can I program Analog Devices' Digital Power products?
FAQ: How close to drop out voltage can one operate an LDO in order to squeeze the last ounce out of my circuits efficiency?
FAQ: How is voltage noise of an LDO measured?
FAQ: Layout of Switching Power Supply
FAQ: Layout recommendations for uPMU/PMU
FAQ: Photosensitive?
FAQ: Powering op-amps (or ADCs) with Dual Supplies
FAQ: Switching Regulators vs LDOs
FAQ: Tips for building the ADIsimPower boards
FAQ: Tips for soldering a LFCSP (QFN) package for a prototype
FAQ: Tips for taking efficiency data
FAQ: Vin range on an Adjustable Output LDO.
FAQ: Where to find package information for ADI parts
Green idle power saving
Half-bridge dc/dc controller
Hand soldering a 12 pin LFCSP
Hand soldering the dual belly pad ADP2384
How are the datasheets split out for these products?
How can I disable one channel when I don't' use it?
How close to drop out voltage can one operate an LDO in order to squeeze the last ounce out of my circuits efficiency?
How close to drop out voltage can one operate an LDO in order to squeeze the last ounce out of my circuits efficiency? (1)
How Do I Generate Negative Supplies?
How does the windowed watchdog operate at power up or after a reset event?
How is the output noise spectral density of a low noise LDO measured?
How is the output noise spectral density of an ultra-low noise LDO measured?
How is the RMS output noise of a low noise LDO measured?
How is the RMS output noise of an ultra-low noise LDO measured?
How much current can the ADN8831 supply to a TEC?
How should I connect ADM2483's Power Valid Pin (PVP) when not using it?
How to handle the sequence in ADP5052?
How to use the ADIsimPower design tools with ADIsimPE integration
Ib +- of Op
Inquiry on MAX Junction Temp Ratings.
Interface box for ADM1062 Sequencer
Is it possible to disable the watchdog functionality if not required?
Is it possible to order a version with factory programmed output voltages?
Is there any guideline for EEPROM programming and factory calibration for ADP1050 and ADP1051?
Isolated DC-DC Power Supply 20W, 36-72V Input , 5V output
Key difference between the ADM268xE and ADM258xE
level of automotive qualification do these parts have?
LT3439 Power Dissipation Calculation
LT8705 alternative
Measuring Signals in a Switching Power Supply
Minimum Load Current Operation - Zero load Operation
Paralleling LDOs to Create More Output Current
Power by Linear Support Community INTRO
Power Management solution for Altera Arria 10 FPGA
Powering Analog circuit through SMPS.
Product Analog Devices USB-SMBUS-CABLEZ.
PWM Setup ZVS app note
Ref design recommendation
selecting an external FET?
soldering temperature and soldering time
Thermal Information
Thermal Information of ADR01TUJZ-EP-R7
Typical markets/applications for this device
USB-SDP-CABLEZ software installer link is broken on User Guide.
Use ADM1062's ADC from inputs VX1-5, VP1-4, VH & Temp sensor without averaging?
Voltage Regulator for 16-bit ADC AD7626
VPx input impedance of ADM1069
What are "Standard models" listed in the datasheets?
What is ADIsimPower?
what is the best digital controller for isolated boost mode current fed converter?
What is the difference between MTBF and MTTF?
What type of passive filters can be added to the output of a linear regulator without causing instability?
What's the ADP3634's internal driver's resistance, Rdson?
What's the big differentiation for ADP5052 in the market?
Where can I find a programming procedure to implement EEPROM programming of ADP1051?
Where can I find the ADP1870 EVB Gerber Files?
Where can I find the Package/Leadframe material information for ADR225HFZ (8 ld Ceramic Flatpack)?
Why would a customer require a windowed watchdog part over a normal watchdog?
ADM1062: Data storage on EEPROM
Q
We would like to use the ADM1062 device in an rugged powersupply and have few
questions to you. 1. The data storage of the EEPROM is approximately 10 Years.
Is it possible to reprogram the EEPROM after it lost the data? 2. Is it
possible at power up first to verrify via SMBus the EEPROM data before the
ADM1062 runs (especially verrify the DAC offest setting)? 3. Is there any other
possibility to reach at least 20 Years data retention?
A
1) The 10 years would be a typical data retention time for EEPROM, depending on
operating conditions of course. After that you'd have to reprogram the part
again to get another 10 (typical) years. If there were any problems programming
the EEPROM that time, then you'd catch it when doing a verify of the EEPROM
write in the programming procedure.
2) In terms of verifying what is programmed into the part at power up, this is
something that can be done across the SMBus interface by a host processor
running suitable code. The default DAC output values could be read and
verified, and the DAC outputs could be enabled at power up in the ADM1062
EEPROM, or they could be enabled by the host processor after the DAC values
have been verified. The state machine in the ADM1062 could be designed so that
it doesn't enable any supplies, and goes into a wait state, where a SMBJump
command is required to move into the power up sequencing states. The host
processor would be able to read the EEPROM contents, verify them, and then
issue the SMJump instruction to continue the power up sequence.
3) As the EEPROM has a limited data retention time, the key thing to do is to
ensure that the memory is 'refreshed', the how and when strategy of the refresh
will probably vary and depend upon the requirements of the application.
adm1062
Share
History
More
Cancel
Comments
Related