Q
The ADM3491 datasheet figure 33 shows the the application circuit for fullduplex
RS485, is it correct to place a resistor Rt between Y and Z ? Usually I would
just
place a Rt on the receiver side not on transmitter side.
A
In a full duplex configuration only the master receiver and most remote slavereceiver need to be terminated. Please see Figure 4 in the attached RS-485/422
Circuit Implementation Guide AN-960.