Q
I have an ADP3040 specified in our schematics, but I can't find that one on
your site. Is the ADP3031 the same thing; Are they completely interchangable?
A
The ADP3040 was a customer specific part. I do not have access to the datasheet
yet - as it was customer specific I doubt I will be able to distribute it.
The ADP3031 should have been the free available version of the ADP3040 - but
the ADP3031 never was released.
Do not distribute this information:
ADP3040 (Step Up, 2MHz PWM Current Mode, Vin=+2.5V to 5.5V, Vout Adj=Vin to 12V
@ Iout=200mA, Iq=5mA, Special for LG Philips Kora, See ADP3031)