No, if the battery termination voltage is above the voltage when it should not be recharged charging stops. There is also temperature supervision of charging which will stop the charging if the temp exceeds JEITA limits. The system can be architected in such a way that the harvested energy can be used by the system if it cannot be used for charging and we have some PMICs which accommodate that.