When EN1 = EN2 = GND, VMPD can be used to go to the lowest ICC consumption mode if RSTMAP is not mapped to any input channel.
The setup is as follows:
EN0 = EN1 = GND
Power up device
VMPD set to ‘1’
VMON[x] set to ‘1’, all channels set to active
RSTMAP[x] set to ‘0’ , no channels mapped to RESET
You can achieve lowest ICC only when RSTMAP is not mapped to any input channel even if VMPD = 1.
The MINIQ board *must* be disconnected.