As long as the total sum of output (LED) current in all strings is 600mA or less, any number of LED strings can be used . There are four current-sink channels into the device that can sink up to 150mA each. If you connect the four sink channels together they can sink 600mA total.