When the load changes from light to heavy, while the input current is less than the Ipeak, the part will work as boost.
When the input current increase further, and the duty cycle up to about 75%, MAX1722x will work as one switch. It will connect the input to output directly.
When the load increases, and the input current is larger than Ipeak, MAX1722x will shut off the output.