Yes. No output voltage information is fed back to MAX77324. Instead, the MAX77324 uses an internal reference voltage of 1V for the TON generator.
The switching frequency is calculated using the following equation: Switching frequency = (Output Voltage /1V) * 2MHz
Example: If the output voltage is set to 1.2V, then the switching frequency will be roughly 2.4 MHz.