Question
Can you let me know the physical dimensions of the ADM7155CP-02-EVALZ board? This no mention of this in the user guide.
Answer
The ADM7155CP-02-EVALZ board dimension is 38.1mm*36.83mm.
ADM7155
Recommended for New Designs
The ADM7155 is an adjustable linear regulator that operates from 2.3 V to 5.5 V and provides up to 600 mA of load current. Output voltages from 1.2 V to...
Datasheet
ADM7155 on Analog.com