Locale Icon
English
EngineerZone
EngineerZone
Power Management
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Power Management
Power Management
Documents Can the MAX17690 in CCM mode?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

MAX17690 Production
The MAX17690 is a peak current mode, fixed-frequency switching controller specifically designed for the isolated flyback topology operating in Discontinuous...
Datasheet
MAX17690 on Analog.com

  • +Power FAQs
  • +AD8240: FAQ
  • +ADIsimPE: FAQ
  • +ADIsimPower: FAQ
  • +ADM1030: FAQ
  • +ADM1031: FAQ
  • +ADM1060: FAQ
  • +ADM1062: FAQ
  • +ADM1064: FAQ
  • +ADM1066: FAQ
  • +ADM1068: FAQ
  • +ADM1069: FAQ
  • +ADM1085: FAQ
  • +ADM1166: FAQ
  • +ADM1171: FAQ
  • +ADM1175: FAQ
  • +ADM1186: FAQ
  • ADM1186: FAQ
  • +ADM1232: FAQ
  • +ADM12914: FAQ
  • +ADM13305-4: FAQ
  • +ADM1816: FAQ
  • +ADM202: FAQ
  • ADM2483_PV pin function
  • +ADM2484e: FAQ
  • +ADM2486: FAQ
  • +ADM2582E: FAQ
  • +ADM2587E: FAQ
  • +ADM2682E: FAQ
  • +ADM2687E: FAQ
  • +ADM3053: FAQ
  • +ADM3054: FAQ
  • +ADM3075E: FAQ
  • +ADM3202: FAQ
  • +ADM3251E: FAQ
  • +ADM3252E: FAQ
  • +ADM3307: FAQ
  • +ADM3483: FAQ
  • +ADM3485E: FAQ
  • +ADM3491: FAQ
  • +ADM4073T: FAQ
  • +ADM483E: FAQ
  • +ADM485: FAQ
  • +ADM6316: FAQ
  • +ADM6320: FAQ
  • +ADM696: FAQ
  • +ADM705: FAQ
  • +ADM706: FAQ
  • +ADM709: FAQ
  • +ADM7151: FAQ
  • +ADM7154: FAQ
  • +ADM7155: FAQ
  • +ADM7170: FAQ
  • +ADM8316: FAQ
  • +ADM869L: FAQ
  • +ADN8831: FAQ
  • +ADP-I2C-USB: FAQ
  • +ADP1043A: FAQ
  • +ADP1046A: FAQ
  • +ADP1047: FAQ
  • +ADP1048: FAQ
  • +ADP1050: FAQ
  • +ADP1051: FAQ
  • +ADP1055: FAQ
  • +ADP1074: FAQ
  • +ADP124: FAQ
  • +ADP125: FAQ
  • +ADP130: FAQ
  • +ADP150: FAQ
  • +ADP1600: FAQ
  • +ADP1607: FAQ
  • ADP160: FAQ
  • +ADP1612: FAQ
  • +ADP1621: FAQ
  • +ADP1741: FAQ
  • +ADP1829: FAQ
  • +ADP1851: FAQ
  • +ADP1870: FAQ
  • ADP195: FAQ
  • +ADP197: FAQ
  • +ADP198: FAQ
  • +ADP2108: FAQ
  • +ADP2118: FAQ
  • +ADP2138CB: FAQ
  • +ADP2140: FAQ
  • +ADP2303: FAQ
  • +ADP2384: FAQ
  • +ADP2386: FAQ
  • +ADP2441: FAQ
  • +ADP2504: FAQ
  • +ADP3040: FAQ
  • +ADP3302: FAQ
  • +ADP3330: FAQ
  • +ADP3338: FAQ
  • +ADP3339: FAQ
  • +ADP3623: FAQ
  • +ADP3624: FAQ
  • +ADP5014ACPZ-R7: FAQ
  • +ADP5046: FAQ
  • +ADP5050: FAQ
  • +ADP5052: FAQ
  • ADP5053: FAQ
  • +ADP5061: FAQ
  • +ADP5090: FAQ
  • +ADP5585: FAQ
  • +ADP5588: FAQ
  • +ADP5589: FAQ
  • +ADP7112: FAQ
  • +ADP7142: FAQ
  • +ADP7182: FAQ
  • +ADR01: FAQ
  • +ADR125: FAQ
  • +ADR127: FAQ
  • +ADR225: FAQ
  • +ADR3450: FAQ
  • +ADR365: FAQ
  • +ADR366: FAQ
  • +ADR381: FAQ
  • +ADR5045: FAQ
  • Can I use LT1640A as AC circuit breaker ?
  • Can I use the Exposed Pad on the MAX256 as the ground terminal?
  • Can the sense resistors in LTC2992 be replaced with a current transformer (CT) sensors?
  • Can you please clarify what to do with the UVLO pin on MAX17613A?
  • +Digital Power: FAQ
  • +DS1233-10+: FAQ
  • +DS1819AR-10-U+: FAQ
  • +DS1831: FAQ
  • +Efficiency Data: FAQ
  • +Generate Negative Supplies: FAQ
  • +Hand Soldering: FAQ
  • How can the residual voltage at the LT1161 output be handled when the device is turned off to prevent unintentional MOSFET switching On?
  • How should I connect ADM2483's Power Valid Pin (PVP) when not using it?
  • How to connect MAX17612 OVLO and UVLO pins when not in use?
  • If Sleep mode is not using, could I leave SL and LED pin floating?
  • In MAX5995C circuit design, for AutoClass function, to further reduce the power consumption, can we connect AUC to Vss to select 5% duty cycle only?
  • +LDO: FAQ
  • +Low Noise: FAQ
  • +LT1161: FAQ
  • LT1640A: FAQ
  • +LT1963: FAQ
  • +LT3045: FAQ
  • +LT3080: FAQ
  • +LT3081: FAQ
  • +LT3092: FAQ
  • +LT3380: FAQ
  • +LT3439: FAQ
  • +LT3508: FAQ
  • +LT3752: FAQ
  • +LT3932: FAQ
  • +LT3950: FAQ
  • +LT4293: FAQ
  • +LT4322: FAQ
  • +LT8277: FAQ
  • +LT8300: FAQ
  • +LT8304: FAQ
  • +LT8306: FAQ
  • +LT8336: FAQ
  • +LT8357: FAQ
  • +LT8361: FAQ
  • +LT8611: FAQ
  • +LT8619: FAQ
  • LT8631EFE#PBF: FAQ
  • +LT8645S: FAQ
  • +LT8646S: FAQ
  • +LT8648S: FAQ
  • +LT8650SHV-CSL#PBF: FAQ
  • +LT8650SP: FAQ
  • +LTC2937: FAQ
  • LTC2937: FAQ
  • +LTC2953: FAQ
  • +LTC2954: FAQ
  • LTC2992: FAQ
  • +LTC3105: FAQ
  • +LTC3114-1: FAQ
  • +LTC3127: FAQ
  • +LTC3221: FAQ
  • +LTC3350: FAQ
  • +LTC3355: FAQ
  • +LTC3588-1: FAQ
  • +LTC3637: FAQ
  • +LTC3643: FAQ
  • +LTC3779: FAQ
  • +LTC3869: FAQ
  • +LTC3897: FAQ
  • +LTC4070: FAQ
  • +LTC4121: FAQ
  • +LTC4231: FAQ
  • +LTC4267-1: FAQ
  • +LTC4267-1: FAQ
  • +LTC4286: FAQ
  • +LTC4292: FAQ
  • LTC4359: FAQ
  • +LTC4364: FAQ
  • +LTC4366: FAQ
  • +LTC4370: FAQ
  • +LTC4370: FAQ
  • +LTC4418: FAQ
  • +LTC4418: FAQ
  • +LTC4421: FAQ
  • LTC4421: FAQ
  • +LTC7890: FAQ
  • +LTC7891: FAQ
  • +LTC9101-1: FAQ
  • +LTC9101-3: FAQ
  • +LTC9111: FAQ
  • LTM2987: FAQ
  • +LTM4638: FAQ
  • +LTM4644: FAQ
  • +LTM4655: FAQ
  • +LTM4661: FAQ
  • +LTM4668A: FAQ
  • +LTM4681: FAQ
  • +LTM4700: FAQ
  • +LTM4705: FAQ
  • +LTM8003: FAQ
  • +LTM8024: FAQ
  • +LTM8042: FAQ
  • +LTM8060: FAQ
  • +LTM8065: FAQ
  • +LTM8078: FAQ
  • +MAX13256ATB+: FAQ
  • +MAX14521E: FAQ
  • +MAX14529E: FAQ
  • +MAX14626ETT+: FAQ
  • +MAX14626ETT+T: FAQ
  • +MAX14655: FAQ
  • +MAX14672ETB+: FAQ
  • MAX14699EWC+: FAQ
  • +MAX14699EWC+: FAQ
  • +MAX14713EWL+: FAQ
  • +MAX14714EWL+: FAQ
  • +MAX14720AEWA+: FAQ
  • +MAX14720EEWA+: FAQ
  • +MAX14721ATP+: FAQ
  • MAX14721ATP+: FAQ
  • +MAX14723ATP+: FAQ
  • +MAX14738EWT+T: FAQ
  • +MAX14750AEWA+: FAQ
  • +MAX14870: FAQ
  • +MAX14870ETC+: FAQ
  • +MAX14871EVKIT#: FAQ
  • MAX14871EVKIT#: FAQ
  • +MAX14874ETC+: FAQ
  • MAX14874ETC+: FAQ
  • +MAX15000AEUB+: FAQ
  • +MAX15003ATM+: FAQ
  • +MAX15004: FAQ
  • +MAX15005AAUA/V+: FAQ
  • +MAX15005AAUE+: FAQ
  • +MAX15005CAUE/V+: FAQ
  • MAX15021: FAQ
  • +MAX15021ATI+: FAQ
  • +MAX15021ATI/V+: FAQ
  • +MAX15023: FAQ
  • +MAX15026BETD+: FAQ
  • +MAX15027ATB+T: FAQ
  • +MAX15032ATA+T: FAQ
  • +MAX15035ETL+: FAQ
  • +MAX15046: FAQ
  • +MAX15058: FAQ
  • MAX15059: FAQ
  • +MAX15059AATE+: FAQ
  • +MAX15059BETE+: FAQ
  • +MAX15062CATA+: FAQ
  • +MAX15066: FAQ
  • +MAX15068ATP+: FAQ
  • +MAX15096AEWE+T: FAQ
  • +MAX15096AGWE+: FAQ
  • +MAX15096AGWE+: FAQ
  • +MAX15096AGWE+T: FAQ
  • MAX15102: FAQ
  • +MAX15102EWL+: FAQ
  • +MAX15108A: FAQ
  • +MAX1510ETB+T: FAQ
  • +MAX15157ATJ+: FAQ
  • +MAX15158: FAQ
  • +MAX1515ETG+: FAQ
  • +MAX15162AATE+: FAQ
  • MAX15162AATG+: FAQ
  • +MAX15162AATG+: FAQ
  • +MAX15301AA02+CJK: FAQ
  • +MAX15301_AA01+CK_A1: FAQ
  • MAX15303: FAQ
  • +MAX15303EVKIT1#: FAQ
  • +MAX15303_AA00+CM_A1: FAQ
  • +MAX1556AETB+: FAQ
  • +MAX1595EUA50+: FAQ
  • +MAX16006BTG+: FAQ
  • +MAX16009TG+: FAQ
  • +MAX16012TT+T: FAQ
  • +MAX16013TT+: FAQ
  • +MAX16025TE+: FAQ
  • +MAX16028TP+: FAQ
  • +MAX16029: FAQ
  • +MAX16046ACB+: FAQ
  • +MAX16046ACB+: FAQ
  • +MAX16046EVKIT+: FAQ
  • +MAX16050ETI+: FAQ
  • MAX16050ETI+: FAQ
  • +MAX16056: FAQ
  • +MAX1605ETT+: FAQ
  • +MAX16061: FAQ
  • +MAX16065: FAQ
  • +MAX16084_XS22B+_A1: FAQ
  • +MAX16122AWT+: FAQ
  • +MAX16125WTEG00+T: FAQ
  • MAX16126 vs MAX16141 ideal diode functionality
  • +MAX16126TCA/V+: FAQ
  • MAX16126_TCA/V+_A1: FAQ
  • +MAX16127TC/V+: FAQ
  • +MAX16141/V+: FAQ
  • +MAX16141/V+T: FAQ
  • +MAX16141/V+T: FAQ
  • +MAX16141AAAF/VY+: FAQ
  • MAX16141AAAF/VY+T: FAQ
  • +MAX16141AAAF/VY+T: FAQ
  • +MAX16141ATD+: FAQ
  • +MAX16141EVKIT#: FAQ
  • MAX16141EVKIT#: FAQ
  • +MAX16141_AAF/V+_A1: FAQ
  • MAX16141_AAF/V+_A1: FAQ
  • +MAX16165: FAQ
  • +MAX16169: FAQ
  • +MAX1634AEAI+: FAQ
  • +MAX16545BGPF+T: FAQ
  • +MAX16550AGPN+: FAQ
  • MAX16550AGPN+: FAQ
  • +MAX16550GPN+T: FAQ
  • MAX16550GPN+T: FAQ
  • +MAX16602GGN+: FAQ
  • +MAX16602GGN+T: FAQ
  • +MAX16602GGN+T: FAQ
  • +MAX16801BEUA+: FAQ
  • MAX16813: FAQ
  • +MAX16813ATP+: FAQ
  • +MAX16813ATP/V+: FAQ
  • MAX16813B: FAQ
  • +MAX16813BATP/V+: FAQ
  • +MAX16814AGP/VY+: FAQ
  • +MAX16814ATP/V+: FAQ
  • +MAX16814AUP/V+T: FAQ
  • +MAX16818: FAQ
  • +MAX16819ATT+: FAQ
  • +MAX16820ATT+: FAQ
  • +MAX16823ATE+: FAQ
  • +MAX16824AUE/V+: FAQ
  • +MAX16826: FAQ
  • +MAX16826ATJ+: FAQ
  • +MAX1682EUK+T: FAQ
  • MAX16833: FAQ
  • +MAX16833AUE/V+: FAQ
  • +MAX16833CAUE/V+CLM: FAQ
  • MAX16838: FAQ
  • +MAX16838BATP/V+: FAQ
  • +MAX1683EUK+T: FAQ
  • +MAX1687ESA+: FAQ
  • +MAX16903: FAQ
  • +MAX16907RATE/V+: FAQ
  • +MAX16910ATA9/V+CB: FAQ
  • +MAX16910CASA9/V+: FAQ
  • +MAX16910EASA8/V+T: FAQ
  • +MAX16930: FAQ
  • +MAX16931AGLR/VY+: FAQ
  • +MAX16935SAUE/V+T: FAQ
  • +MAX16936EVKIT#: FAQ
  • +MAX16946: FAQ
  • +MAX16956AUBA+: FAQ
  • +MAX16956AUBA/V+: FAQ
  • +MAX16961: FAQ
  • +MAX1698AEUB+: FAQ
  • MAX16990: FAQ
  • +MAX16990ATCC/V+: FAQ
  • +MAX16992ATCC/V+: FAQ
  • +MAX16993AGJF/VY+: FAQ
  • +MAX16998AATA+: FAQ
  • +MAX16999AUA05+: FAQ
  • +MAX17000AETG+: FAQ
  • +MAX1701EEE+: FAQ
  • +MAX17075: FAQ
  • +MAX1708EEE+: FAQ
  • MAX17105ETG+: FAQ
  • +MAX17105ETG+_T1: FAQ
  • +MAX17135ETJ+: FAQ
  • MAX17220: FAQ
  • MAX17220ALT+: FAQ
  • +MAX17220ALT+T: FAQ
  • +MAX17220ELT+T: FAQ
  • +MAX17221ELT+: FAQ
  • MAX17222: FAQ
  • +MAX17222ALT+: FAQ
  • MAX17222ELT+: FAQ
  • +MAX17222ELT+T: FAQ
  • +MAX17223: FAQ
  • +MAX17224ALT+: FAQ
  • +MAX17225ALT+: FAQ
  • +MAX17225ELT+: FAQ
  • MAX17225ENT+: FAQ
  • +MAX17225ENT+T: FAQ
  • +MAX17227AANT+: FAQ
  • +MAX17227AATA+: FAQ
  • +MAX17245ETERA+: FAQ
  • +MAX1724EZK30+: FAQ
  • MAX17250ANC+: FAQ
  • +MAX17250ANC+T: FAQ
  • +MAX17270ENE+: FAQ
  • +MAX17270_NE+_A1: FAQ
  • +MAX17290ETCC+: FAQ
  • MAX17292: FAQ
  • +MAX17292ETCF+: FAQ
  • +MAX17335X2EVKIT#: FAQ
  • +MAX1742: FAQ
  • +MAX1744: FAQ
  • +MAX17498BATE+: FAQ
  • MAX17501: FAQ
  • +MAX17501ATEVKIT#: FAQ
  • +MAX17502EATB+: FAQ
  • +MAX17502FATB+: FAQ
  • +MAX17502GATB+T: FAQ
  • +MAX17502HAUD+: FAQ
  • +MAX17503ATP+: FAQ
  • MAX17504: FAQ
  • +MAX17504AATP+: FAQ
  • +MAX17504ATP+: FAQ
  • +MAX17504A_TP+_A1: FAQ
  • MAX17505: FAQ
  • +MAX17505ATP+: FAQ
  • +MAX17509: FAQ
  • +MAX17523ATE+: FAQ
  • +MAX17525ATP+: FAQ
  • +MAX17526AATP+: FAQ
  • +MAX17526AATP+: FAQ
  • +MAX17531: FAQ
  • +MAX17536: FAQ
  • +MAX17541GATB+: FAQ
  • +MAX17544ATP+: FAQ
  • +MAX17546ATP+_T1: FAQ
  • MAX17552: FAQ
  • +MAX17552AATB+: FAQ
  • +MAX17552ATB+T: FAQ
  • +MAX17552A_UB+_A1: FAQ
  • +MAX17557: FAQ
  • +MAX17558ATJ+: FAQ
  • +MAX17559_CJ+_A1: FAQ
  • +MAX17561AUD+: FAQ
  • +MAX17563AUD+: FAQ
  • MAX17563AUD+: FAQ
  • MAX17572: FAQ
  • +MAX17572ATC+: FAQ
  • MAX17574ATG+: FAQ
  • +MAX17574ATG+T: FAQ
  • +MAX17580ATC+: FAQ
  • +MAX17595ATE+: FAQ
  • MAX17596ATE+: FAQ
  • +MAX17596ATE+T: FAQ
  • +MAX17597ATE+: FAQ
  • +MAX17598: FAQ
  • MAX17599ATE+: FAQ
  • +MAX17599ATE+T: FAQ
  • +MAX17600ASA+: FAQ
  • +MAX17601ASA+: FAQ
  • +MAX17606: FAQ
  • +MAX17608: FAQ
  • +MAX17608ATC+: FAQ
  • +MAX17609: FAQ
  • +MAX17612AATB+: FAQ
  • +MAX17613AATP+: FAQ
  • MAX17613A_TP+_A1: FAQ
  • +MAX17613BATP+: FAQ
  • +MAX17616A: FAQ
  • +MAX17630: FAQ
  • +MAX17633AATP+: FAQ
  • +MAX17651AZT+: FAQ
  • MAX17681: FAQ
  • +MAX17681AATB+: FAQ
  • +MAX17681ATB+: FAQ
  • +MAX17681A_TB+_A1: FAQ
  • MAX17682: FAQ
  • +MAX17682ATP+: FAQ
  • -MAX17690ATE+T: FAQ
    • Can the MAX17690 in CCM mode?
    • Does MAX17690 has a Eutectic Die Attach?
    • How to get the SIMPLIS models of Maxim's power devices?
    • In the MAXREFDES1105, why is a 33mOhm current sense resistor used?
    • In the MAXREFDES1175 a 62mOhm current sense resistor was calculated, why was a 60mOhm resistor used?
    • In the MAXREFDES1177 a 61mOhm current sense resistor was calculated, why was a 60mOhm resistor used?
    • Is it possible to get the datasheet of the custom transformers used in new reference designs?
    • Using a Kelvin current sense resistor with the MAX17690, should I connect the pins to signal ground or power ground?
    • When designing with the MAX17690 device, which value for the maximum CS current limit threshold should I use?
    • When is the feedback voltage sampled on the MAX17690?
    • Why MAX17690 EESIM simulation restricting Vout to 48V?
  • +MAX17690ATE/V+: FAQ
  • +MAX17710GB+: FAQ
  • +MAX1771ESA+: FAQ
  • +MAX17761: FAQ
  • +MAX18166: FAQ
  • +MAX1836EUT50#TG16: FAQ
  • +MAX1846EUB+: FAQ
  • +MAX1847: FAQ
  • MAX1896: FAQ
  • +MAX1896EUT+: FAQ
  • +MAX1932: FAQ
  • +MAX1945REUI+: FAQ
  • +MAX1951AESA+T: FAQ
  • +MAX1957EUB+: FAQ
  • +MAX19708: FAQ
  • +MAX20002: FAQ
  • +MAX20003C_TPA/VY+_A1: FAQ
  • MAX20004: FAQ
  • +MAX20004AFOA/VY+: FAQ
  • +MAX20004AFOC/VY+: FAQ
  • +MAX20004_FOB/VY+_B1: FAQ
  • +MAX20006AFDB/V+_T1: FAQ
  • +MAX20008AFOA/VY+_T1: FAQ
  • +MAX20012BATJL/V+T: FAQ
  • MAX20022: FAQ
  • +MAX20022ATIA+: FAQ
  • +MAX20022ATIA/V+: FAQ
  • +MAX20029ATIA/V+: FAQ
  • +MAX20029_TIA/V+_A1: FAQ
  • MAX20034ATI/VY+: FAQ
  • +MAX20034ATI/VY+_T1: FAQ
  • +MAX20034ATIR/VY+: FAQ
  • +MAX20040EVKIT#: FAQ
  • +MAX20048ATGA/VY+: FAQ
  • +MAX20050ATC/V+: FAQ
  • +MAX20050EVKIT#: FAQ
  • +MAX20051AAUD/V+: FAQ
  • +MAX20056BAUGA/V+: FAQ
  • +MAX20057ATIA/VY+T: FAQ
  • +MAX20059ATCA/VY+: FAQ
  • MAX20067GTJ/V+: FAQ
  • +MAX20067GTJ/V+T: FAQ
  • +MAX20070BGTJ/V+: FAQ
  • +MAX20075ATC/V+_T1: FAQ
  • +MAX20075ATCA/V+: FAQ
  • +MAX20075EVKIT#: FAQ
  • +MAX20076ATC/V+: FAQ
  • +MAX20076ATCA/V+: FAQ
  • +MAX20077ATCA/VY+: FAQ
  • +MAX20078ATE+: FAQ
  • +MAX20078ATE/V+T: FAQ
  • +MAX20078ATE/VY+T: FAQ
  • +MAX20078_TE+_A1: FAQ
  • +MAX20078_TE/V+_A1: FAQ
  • +MAX20090ATP/V+: FAQ
  • +MAX20090ATP/VY+: FAQ
  • +MAX20090BATP/V+: FAQ
  • +MAX20092ATJ/VY+: FAQ
  • +MAX20098ATE/V+: FAQ
  • +MAX20098ATEA/V+: FAQ
  • +MAX20098ATEA/VY+: FAQ
  • +MAX20098ATED/VY+: FAQ
  • +MAX20098ATEF/VY+: FAQ
  • +MAX20323AENC+: FAQ
  • +MAX20323AENC+: FAQ
  • +MAX20323CENC+T: FAQ
  • +MAX20323DENC+T: FAQ
  • MAX20323DENC+T: FAQ
  • +MAX20328AEWA+: FAQ
  • MAX20330AEVKIT#: FAQ
  • +MAX20330AEWA+: FAQ
  • +MAX20331AEWL+: FAQ
  • +MAX20331AEWL+: FAQ
  • +MAX20343BEWE+: FAQ
  • MAX20361AEWC+: FAQ
  • +MAX20361AEWC+_B1: FAQ
  • +MAX20410AFOA/VY+: FAQ
  • +MAX20419ATGA/V+: FAQ
  • +MAX20480ATEA/VY+: FAQ
  • +MAX20710EPL+T: FAQ
  • +MAX20730EPL+: FAQ
  • +MAX20733: FAQ
  • +MAX20734EPL+: FAQ
  • +MAX20735: FAQ
  • +MAX20743EPL+: FAQ
  • MAX20751: FAQ
  • MAX20751EKX+: FAQ
  • +MAX20751EKX+T: FAQ
  • +MAX20754ETMA1+: FAQ
  • +MAX20801AEVKIT#: FAQ
  • +MAX20801TPBA+: FAQ
  • +MAX20801TPBD+: FAQ
  • +MAX20812: FAQ
  • +MAX22201: FAQ
  • +MAX22256: FAQ
  • +MAX25203: FAQ
  • +MAX25206ATPA/VY+: FAQ
  • +MAX25210ASA8/V+: FAQ
  • +MAX25221BATJ/V+: FAQ
  • +MAX25240: FAQ
  • +MAX25254: FAQ
  • +MAX25262: FAQ
  • MAX253ESA+: FAQ
  • +MAX253ESA+: FAQ
  • +MAX25601AATJ/VY+: FAQ
  • +MAX25610AATE/VY+T: FAQ
  • +MAX25611AATC/VY+: FAQ
  • +MAX25611DATC/VY+: FAQ
  • MAX256ASA+: FAQ
  • +MAX31740ATA+: FAQ
  • +MAX31760AEE+: FAQ
  • +MAX31760AEE+T: FAQ
  • MAX31785: FAQ
  • +MAX31785: FAQ
  • +MAX31785AETL+T: FAQ
  • +MAX31785AETL+T: FAQ
  • +MAX31790ATI+: FAQ
  • +MAX31790ATI+T: FAQ
  • MAX31790ATI+T: FAQ
  • +MAX34440ETLA1+: FAQ
  • +MAX34446ETL+T: FAQ
  • +MAX34451ETNA1+: FAQ
  • +MAX34451ETNA2+: FAQ
  • +MAX34451ETNA3+: FAQ
  • +MAX38640AELT+: FAQ
  • MAX38643AELT+: FAQ
  • +MAX38643AELT+T: FAQ
  • +MAX38643AENT+T: FAQ
  • +MAX38886ATD+: FAQ
  • MAX38888ATD+: FAQ
  • +MAX38888ATD+T: FAQ
  • +MAX38889AATE+: FAQ
  • +MAX38902AATA+: FAQ
  • +MAX38902EVKIT#: FAQ
  • +MAX38903AANL+: FAQ
  • +MAX38908ANL+: FAQ
  • +MAX40200: FAQ
  • +MAX40200ANS+: FAQ
  • +MAX40200AUK+: FAQ
  • +MAX40200AUK+T: FAQ
  • +MAX40203ANS+: FAQ
  • +MAX40203ANS+T: FAQ
  • +MAX4370: FAQ
  • +MAX4427MJA/883B: FAQ
  • +MAX4428ESA+: FAQ
  • +MAX44299: FAQ
  • +MAX4820ETP+: FAQ
  • +MAX4821: FAQ
  • +MAX4821: FAQ
  • +MAX4896ATP+: FAQ
  • +MAX4896ATP+: FAQ
  • +MAX4915AELT+: FAQ
  • +MAX5033: FAQ
  • MAX5035: FAQ
  • +MAX5035AASA+: FAQ
  • +MAX5035EASA/V+T: FAQ
  • +MAX5048: FAQ
  • +MAX5048CAUT+: FAQ
  • +MAX5082: FAQ
  • +MAX5084ATT+T: FAQ
  • +MAX5085ATT+: FAQ
  • +MAX5902AAEUT+: FAQ
  • +MAX5903AAETT+: FAQ
  • +MAX5903AAETT+: FAQ
  • +MAX5921FESA+: FAQ
  • +MAX5943AEEE+: FAQ
  • +MAX5947BESA: FAQ
  • +MAX5954AETX+: FAQ
  • MAX5954AETX+: FAQ
  • +MAX5954LETX+: FAQ
  • +MAX5965A: FAQ
  • +MAX5969AETB+: FAQ
  • MAX5969AETB+: FAQ
  • +MAX5969BETB+: FAQ
  • +MAX5969BEVKIT+: FAQ
  • +MAX5971AETI+: FAQ
  • +MAX5971BETI+: FAQ
  • +MAX5974AATE+T: FAQ
  • +MAX5974CETE+: FAQ
  • MAX5974CETE+: FAQ
  • +MAX5974D: FAQ
  • MAX5974DATE+: FAQ
  • +MAX5974DATE+: FAQ
  • +MAX5974EETE+: FAQ
  • +MAX5977AETP+: FAQ
  • +MAX5980AGTJ+: FAQ
  • +MAX5991AETP+: FAQ
  • +MAX5995AATE+: FAQ
  • +MAX5995AETE+T: FAQ
  • MAX5995B: FAQ
  • MAX5995BATE+: FAQ
  • +MAX5995CETE+: FAQ
  • +MAX618EEE+: FAQ
  • +MAX6301: FAQ
  • +MAX6335: FAQ
  • +MAX6340_UK16+_A1: FAQ
  • +MAX634MJA/883B: FAQ
  • MAX6369: FAQ
  • +MAX6369KA+T: FAQ
  • +MAX6381XR26D3/V+T: FAQ
  • +MAX6389_XS16D3_A1: FAQ
  • MAX6412: FAQ
  • +MAX6412_UK16+_A1: FAQ
  • +MAX6420UK29+T: FAQ
  • +MAX6425: FAQ
  • +MAX6443: FAQ
  • +MAX6461: FAQ
  • MAX6495: FAQ
  • +MAX6495: FAQ
  • +MAX6496ATA/V+: FAQ
  • +MAX651MSA/PR+_T1: FAQ
  • +MAX6615AEE+: FAQ
  • +MAX6615AEE+: FAQ
  • +MAX6615AEE: FAQ
  • +MAX6639: FAQ
  • MAX6639: FAQ
  • +MAX6639FAEE: FAQ
  • +MAX6641: FAQ
  • +MAX6641: FAQ
  • +MAX6643LBBAEE+: FAQ
  • +MAX6650EUB+: FAQ
  • MAX6650EUB+: FAQ
  • +MAX6653AEE+: FAQ
  • MAX6684ESA+: FAQ
  • +MAX6684ESA+: FAQ
  • +MAX668EUB+: FAQ
  • +MAX668EUB_T1: FAQ
  • +MAX668EVKIT+: FAQ
  • +MAX6710KUT+: FAQ
  • +MAX6719AUTSVD3+T: FAQ
  • +MAX6722UTSDD3+: FAQ
  • +MAX6735A: FAQ
  • +MAX6735_KASYD3+_A1: FAQ
  • +MAX6747: FAQ
  • +MAX6753: FAQ
  • +MAX6759: FAQ
  • +MAX6764UT+: FAQ
  • MAX680CSA+: FAQ
  • +MAX6816: FAQ
  • +MAX6842DUKD0+T: FAQ
  • +MAX6867: FAQ
  • +MAX6895AALT+: FAQ
  • +MAX6895AAZT/V+T: FAQ
  • +MAX6975ATL+: FAQ
  • +MAX700CPA+: FAQ
  • +MAX705ESA+: FAQ
  • MAX706: FAQ
  • +MAX706SESA: FAQ
  • +MAX77324EWT00+: FAQ
  • +MAX77324EWTAD+: FAQ
  • +MAX774ESA+: FAQ
  • MAX77501EWV+: FAQ
  • +MAX77501EWV+T: FAQ
  • +MAX77503AEWC+T: FAQ
  • +MAX77503BEWC18+: FAQ
  • +MAX77504AAFC+T: FAQ
  • +MAX77542: FAQ
  • +MAX77597EVKIT#: FAQ
  • MAX775: FAQ
  • +MAX77643AANA+: FAQ
  • +MAX77655EWE+T: FAQ
  • +MAX77686: FAQ
  • +MAX77714EWC+: FAQ
  • +MAX77752AETL+: FAQ
  • +MAX77756: FAQ
  • +MAX77801ETP+: FAQ
  • +MAX77801_TP+_A1: FAQ
  • +MAX77812 EVALUATION KIT SOFTWARE: FAQ
  • +MAX77812AEWB+: FAQ
  • +MAX77812BEWB+: FAQ
  • +MAX77812CEWB+T: FAQ
  • MAX77812EWB+: FAQ
  • +MAX77812EWB+T: FAQ
  • +MAX77813EWP+: FAQ
  • +MAX77816AEWP+: FAQ
  • +MAX77816CEWP+T: FAQ
  • +MAX77827AEFD+_T1: FAQ
  • +MAX77827AEWC+: FAQ
  • +MAX77837: FAQ
  • +MAX77839: FAQ
  • +MAX77863AEWJ+: FAQ
  • +MAX77874: FAQ
  • +MAX786: FAQ
  • +MAX797MJE: FAQ
  • +MAX813LCPA: FAQ
  • +MAX8212CPA+: FAQ
  • +MAX821LUS+T: FAQ
  • +MAX823L: FAQ
  • +MAX823TEUK+: FAQ
  • +MAX824: FAQ
  • +MAX834EUK+: FAQ
  • +MAX8535: FAQ
  • +MAX8556ETE+: FAQ
  • +MAX8559ETAAJ+: FAQ
  • +MAX8569AETT+: FAQ
  • +MAX8570ELT+: FAQ
  • +MAX8570EUT+: FAQ
  • +MAX8597ETP+: FAQ
  • +MAX8607ETD+: FAQ
  • +MAX860MSA/PR2+_T1: FAQ
  • +MAX8625AETD+: FAQ
  • +MAX8647ETE+: FAQ
  • +MAX8664: FAQ
  • +MAX8668: FAQ
  • +MAX8686ETL+: FAQ
  • +MAX8794ETB+: FAQ
  • +MAX8815AETB+T: FAQ
  • +MAX8840ELT18+: FAQ
  • +MAX8858ETJ+: FAQ
  • +MAX8869EUE18+: FAQ
  • +MAX8881: FAQ
  • +MAX8887EZK18+T: FAQ
  • +MAX8892: FAQ
  • +MAX889RESA+: FAQ
  • +MAX8902AATA+: FAQ
  • +MAX8902AATA/V+: FAQ
  • +MAX8902B: FAQ
  • MAX8969AEWL53+: FAQ
  • +MAX8969AEWL53+T: FAQ
  • +MAXM15064AMB+T: FAQ
  • +MAXM15462AMB+: FAQ
  • +MAXM17502EVKIT#: FAQ
  • +MAXM17503ALJ+: FAQ
  • +MAXM17504EVKITAE#: FAQ
  • +MAXM17505: FAQ
  • +MAXM17515: FAQ
  • MAXM17532: FAQ
  • +MAXM17532AMB+T: FAQ
  • MAXM17537ALY#: FAQ
  • +MAXM17537ALY#T: FAQ
  • +MAXM17544ALJ+: FAQ
  • +MAXM17544EVKIT#: FAQ
  • MAXM17545: FAQ
  • +MAXM17545ALJ+T: FAQ
  • +MAXM17552: FAQ
  • +MAXM17575ALI#T: FAQ
  • +MAXM17575EVKIT#: FAQ
  • +MAXM17623AMB+T: FAQ
  • +MAXM17624AMB+: FAQ
  • +MAXM17635AMG+: FAQ
  • +MAXM17761ALI+: FAQ
  • +Measuring Signals: FAQ
  • +Package Information: FAQ
  • +Photosensitive: FAQ
  • +Power Management Support Intro: FAQ
  • +Switching Power: FAQ
  • +Temperature Grade: FAQ
  • +uPMU: FAQ
  • +VT1697SBFQX: FAQ
  • What is the maximum current the flag pin on the MAX17613A can sink?
  • When using two LTC4359 controllers with different input voltages, why does the high-side MOSFET turn off during source transition?
  • Where can I get the LTC9101-3 software interface datasheet?
  • Where can I get the LTM2987BY datasheet from?
  • Why does the MAX5995B on the MAXREFDES1266 consume 13mA even at light loads?

Can the MAX17690 in CCM mode?

Answer is no (cannot operate in CCM).
The MAX17690 is a peak current mode, fixed-frequency switching controller specifically designed for the isolated Fly Back topology operating in Discontinuous Conduction Mode (DCM). The device senses the isolated output voltage directly from the primary-side Fly Back waveform during the off-time of the primary switch.
Device samples the reflected output voltage information on the primary winding during the time when the primary NMOSFET is turned-off, and energy stored during the on-time is being delivered to the secondary.
The sampling takes place when the secondary current is near to zero to nullify any effect of forward voltage drop of the rectifier diode.
MAX17690 is designed to work in DCM mode and can NOT be used in CCM mode.
Tags: MAX17690 flyback switching regulators Forward MAX17690ATE+T 000097172 and Isolated Controller Show More