What is the NVM programming for the MAX20751, MAX15301 and MAX15303?
Q1) How many times can the STORE_USER_ALL command be executed (to save the user configuration inside the OTP)? Answer: Up to 4 times.
Q2) Is the max-4-time write limitation for the OTP applicable to the MAX15301 and MAX15303? Answer:The MAX15301 and MAX15303 utilize flash memory, so they do not have any practical limitation on the number of times that STORE_USER_ALL or STORE_DEFAULT_ALL can be sent.
Q2) How long is the expected/guaranteed retention of the data stored in the MAX20751 OTP? 10 years? Answer: Data Retention: >10 Years at 85°C