Post Go back to editing

ADM811TARTZ WHITH POWER FAIL

ADM811TARTZ is perfect as Logic Low RESET for ADAU1701 and I use it in different hardware.
I have to modify a hardware with on board ADAU1701 and I need an IC identical to ADM811TARTZ but with integrated also the function POWER FAIL INPUT, to check the level of battery charge.
I do not need to constantly know the charge, but only a level and exactly when the battery reaches the minimum level allowed.
In an old circuit I used the POWER FAIL INPUT of an ADM706 connected as shown in the drawing and it works perfectly.

Some advice, thank you

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.