Post Go back to editing

I would like to ask about the input voltage of the LT3090.

Hello. I am a graduate student studying at Chungbuk National University in South Korea.

Nowaday, I used the LT3090 and I made it according to the configuration of the Basic Adjustable Regulator described in Datasheet.

But I did not see the input voltage on the data sheet up to -10V. So I entered -15V with my fault. IC seems to be broken.

The Floating 3-Terminal Adjustable Regulator on the datasheet shows only input voltages from -17V to -22V.

Does the LT3090 have input voltages below -10V? I wonder.

If I can input a voltage below -10V, how should I configure it?
  • This is what I normally tell people so they will be ready to work with LDOs: 

    NOTE WHEN WORKING WITH LDOS (written for positive LDOs but in general applies to negative LDOs as well):  An input voltage that is too close to the programmed output voltage (too low) may cause dropout operation and a loss of output voltage regulation.  An input voltage that is too high above the output may increase power dissipation to an unacceptable level.  Finally, a protection feature within the LT3090 reduces output current capability at higher input voltages.

     

     

    The image below shows the circuit that you mentioned - The Basic Adjustable Regulator:

    VIN of the Basic Adjustable Regulator shown above is limited to 10V because

    1. my general comments about LDO power dissipation above and
    2. the LT3090 has reduced output current capability (also mentioned above) for larger VIN to VOUT differentials according to the Internal Current Limit curve shown below from the datasheet.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.