LT8302或者LT8304 设计问题

hello

请问我要设计一个反激DCDC拓扑的10W的小电源,想用LT8302或者LT8304,我的输入条件是VIN=16~40DC,输出是vout=8V, Iout=1.25A; 按照之前设计经验算的匝比是n=1.2(Dmax=0.4, VIN_min*Dmax/{(vo+vf)*(1-Dmax)}; Lp=4uH(vin_min*Dmax/detal_I; detal_I=2*Iav/Dmax);  而按照LT8304的设计工具计算的匝比却是3.81,感量是17.33;请问这个是怎么计算的?因为这个是内置的MOS,电流最大是2A,实际原边峰值电流按照LT8304计算出的电流是1.93A, 这个余量够吗?LT3748是否也可以,如有合适的方案请推荐

Parents Reply Children
No Data