Post Go back to editing

ADP2442 buck-boost simulation in LTSpice

Hello,

I am trying to simulate a buck-boost converter from 12V to -10V. I use the ADP2442 regulator model provided by the latest LTSpice version.

The output ramps down but then it flattens out at approximately -5.6V. I tried changing the feedback divider for other than -10V outputs but without results. As long as the output voltage set by feedback is above -5.6V (e.g. -4V) the supply works fine. This all happens with no load. For a load switch the supply enters in a current limiting mode precisely regulating the output voltage to Iout*Rout (about -4.4V=-550mA*8ohms) and continues switching without hiccups. The regulated current limit is far from the overcurrent condition.

Any possibility to have a bug in the ADP2442 model or am I missing something in the simulation? It should be noted that the exact same design has been built on PCB and is working without issues to output voltages down to -16V.

Please see the schematic attached for reference.

Thanks, Gabor

vpsm_fixed.asc.zip