Hello! I am working with a LTC4001 along with a Panasonic 20700 battery and am having some issues. The part will start up and I can see the switching begin while the current ramps up to charge the battery - but then everything stops and the part resets. If you probe the softstart line, it looks like a sawtooth with it coming up appropriately but then shutting back down. Attached is the schematic. I have tried dropping the input and output capacitors down to the 10uF minimums as well with the same results. Hopefully its something dumb I have done, help!
Notes : I do not want temperature monitoring involved, I would like the battery to charge at 2A, and flag me that the charging is complete when the charge current gets to 80mA or below.
Thank you!