Hello,
My customer is reviewing to use LTM4611 in their product.
For this, they are considering the heating condition of LTM4611.
Q1) Would you provide materials (simulation/test result/......) about the heating/radient condition of LTM4611?
And they will use a heatsink (375424B00034G of AAVID compamy) which is recommended by ADI(LTC).
So they want to know if they only add this heatsink to LTM4611, they can get a stable power supply and reduce power consumption.
- Their Max. load conditions are like below.
1. Input 4V
2. Output 2V and 11A
Q2) Would you advise whether they can get a stable power only to add a heatsink (your recommended in Datasheet)?
Q3) Would you provide materials (simulation/test result/......) about the heating/radient condition of LTM4611 at their max. load condition?
Please advise me.
Regards,
Se-woong