Post Go back to editing

Are there models of ADP1074 and ADP1071-2 for LTSPICE available?

Are these models available?  If not what would be the closest part that I can use?  Also do you have any suggested reading on synchronous flyback vs synchronous forward (with active clamp) topologies?  I am trying to decide which most appropriate for this design.  It would be good to find some info which helps you choose appropriate parts for the power stage (transformer, mosfets ect).

Thanks,

Dan Baldor

Parents
  • The ADP1071-2 will indeed be a good fit for this. The ADP1071-2 is in pre-release status so the full datasheet is not yet available. However, it is exactly similar to ADP1074 (active clamp forward converter) with fewer pins. I suggest you contact the local FAE/Sales to get samples. In the meantime I have attached the some data for a design that is rated at 36-60Vin, 12Vout, 3A nominal (5A peak).

    Lt Comm Data

Reply
  • The ADP1071-2 will indeed be a good fit for this. The ADP1071-2 is in pre-release status so the full datasheet is not yet available. However, it is exactly similar to ADP1074 (active clamp forward converter) with fewer pins. I suggest you contact the local FAE/Sales to get samples. In the meantime I have attached the some data for a design that is rated at 36-60Vin, 12Vout, 3A nominal (5A peak).

    Lt Comm Data

Children
No Data