Hello all,
first time poster here, so I am not sure if this ends in the right forum:
I am working with some poer regulators: LDO type, positive and negative:
ADP7118 and ADP7182 in SOT23-5 Package, just for some information. Adjustable versions
Now I am having trouble to follow the datasheets in regard of the noise reduction techniques.
page 16 ( on Rev D datasheet)
noise = 11uV * (Rparallel + R2)/R2; this one is kind of understandable ( its for the positive LDO)
now regarding the negative LDO, suddenly there appear to be 2 formulas, one is just describes in textform? what is that about, the other one has the same reading but suddenly is slightly different and in the text it says:
The noise of the LDO is approximately the noise of the fixed outputLDO (typically 18 µV rms) times RFB2, divided by the parallelcombination of RNR and RFB1
The noise of the LDO is approximately the noise of the fixed outputLDO (typically 18 µV rms) times the high frequency ac gain
now is that supposed to be the same, those two sentences ( simply someone forgot to dlete one after reviweing it
those two statement dont make any sense in combination, either the first one is adifferent noise, for example fixed output vs adjustable output, but two noises for one and the same thing, cannot exist.
So I would appreciate any further explanation, since i cannto explain this any more
Thanks a lot for reading,
cheers
Hi Mex,
The statement:
"The noise of the LDO is approximately the noise of the fixed output LDO (typically 18 µV rms) times the high frequency ac gain" is correct. At high frequency operation, Xcnr is almost negligible on the equation compared to RFB1. The simplified equation should give you equation #2 on the data sheet.
AC gain = {[Rfb1 // (RNR +Xcnr)] + Rfb2} /Rfb2 ; RNR >> Xcnr; Xcnr is negligible.
Simplified equation:
AC gain = [(Rfb1 // RNR) + Rfb2] / Rfb2 which when further simplied is equal to equation #2.
"The noise of the LDO is approximately the noise of the fixed output LDO (typically 18 µV rms) times RFB2, divided by the parallel combination of RNR and RFB1" is incorrect and should reflect same equation as the ADP7118 (positive LDO) equation #9. We'll update the data sheet to reflect the correct description of the equation.
Basically equation#9 of the ADP7118 datasheet equates to the noise of fixed output multiplied by the AC gain since at high frequency Xcnr is negligible for the AC gain.
Thanks,
Alex