Buck ic for 320Vout application

Hello,

Im searching a controller for high voltage buck.

500V:400V input -> 320V output. 300Khz-400Khz freq. 2KW.

i need also output current regulation as current limit...

I thought about LT3840 (with external drivers off course) but i know that i will have some problems with output current measure and current regulation due to the extream voltage.

1.  There any other option connecting the current measurement resistor except in series with inductor? mabe somehow with current transformer? 

2. Is there any other IC that fit for this app? i thought about lt3741 because of the Average Current Mode but this ic demand 2V at VIN above the output voltage - again, its not possible.

  • 0
    •  Analog Employees 
    on Jun 25, 2018 8:57 PM over 2 years ago

    Thanks for the post.

    I'm the applications engineer for the LT3741 and I agree it is not a great starting point for your design requirements.

    I thought about this and my best advice would be for you to do a web search on "resonant full bridge reference design" or something similar, and if you are fortunate something close to what you need will come up.

  • 0
    •  Analog Employees 
    on Jun 26, 2018 3:03 AM over 2 years ago

    Hello

    If the source return can float with respect to the 320V return, and a non-synchronous converter is acceptable, you could use a LT3825 to make a negative buck converter on the return side. Feedback and Vcc come from a second winding on the inductor. For 2kW, you will need to add a driver stage.

    Regards

    David

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:06 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin