Post Go back to editing

LT3042 PG pin maximum current

Thread Summary

The user inquired about the maximum current allowed through the open collector PG pin, which is not specified in the datasheet. The support engineer provided a curve showing the relationship between the sinking current Ipg and the logic voltage level Vpg, indicating that for a logic low level of 0.5V, the PG current is approximately 1.1mA.
AI Generated Content

What is the maximum current allow through the open collector PG pin? Nothing is stated in the datasheet. It looks like 100uA has been used for curves and examples.