Hi all, I am doing research for system ID for battery systems and I need to measuring a single cell voltage and set the discharge state of the balancing resistor at rate of less than 1 ms. My current set up is a laptop connected through a serial port to a LTC DC2026 Demo board connected to a LTC DC2259 battery stack monitor. Right now I am capable of doing this in about 2.4 ms and I believe that the majority of this time is used up in communication of data between the two demo boards and the serial communication to a laptop. Is there a way to speed up this process. Again I am only interested in a single cell. Thanks for the help.